Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Powering Arduino Uno Through different inputs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 27 replies
  • Subscribers 415 subscribers
  • Views 9417 views
  • Users 0 members are here
  • arduino uno
  • power
  • arduino
  • beginner
Related

Powering Arduino Uno Through different inputs

Adam_A
Adam_A over 3 years ago

Hello, recently I have been doing a project on an Arduino Uno that uses the display, however due to the limited space I have in my project build im unable to plug in power using the normal Usb option and 12v Barrel jack, the only way I could power it is I can wire power from a power supply to the Arduino Uno, I'm aware that I can use the inputs over here (on the power rail) to wire power to the Arduino (Refer to image 1) 

image 1

image

However all of these inputs are occupied and it isn't possible for me to input power from there, so now we are left with the empty slots refer to image 2 (empty slots are highlighted in yellow) 

Image 2

image

My question is that are we able to wire 5V power from the Arduino power Supply (refer to image 3 for power supply) then to the Arduino Uno highlighted yellow slots?? 

Image 3

image 

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Adam_A +1 verified
    I'd go for these two solder holes (corrected after being reminded by @beacon_dave that VIN is before the regulator)
Parents
  • Andrew J
    0 Andrew J over 3 years ago

    That's not an Arduino Uno form I've seen before with the 12 hole block or the holes in front of the standard headers.  Also, in the small yellow box on the bottom edge, mine is marked IOREF where yours is marked 5V.  Can you give more details on this board: manufacturer etc.  Are they actual holes in front of the headers or is it just the photo?  I assume image 3 is showing a board you want to use to route 5V and GND (don't forget this!) to the Arduino board and isn't actually plugged into the Arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Adam_A
    0 Adam_A over 3 years ago in reply to Andrew J

    Yeah mine is a bit different thus I am struggling to find any guides mentioning my specfic board (i found an aliexpress link with the same model i have or what looks like it) https://www.aliexpress.com/item/1005004697397154.html?channel=twinner I'm not sure what it is exactly since I received that part from my school and didn't purchase it directly.

    And yeah I was wondering if I would have any success plugging in power from the 12 hole block. And no the power supply isn't plugged in to the Arduino, here is a picture of the display and Arduino plugged in 

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    +1 Jan Cumps over 3 years ago in reply to Adam_A

    I'd go for these two solder holes (corrected after being reminded by @beacon_dave that VIN is before the regulator)

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Adam_A
    0 Adam_A over 3 years ago in reply to Jan Cumps

    Yeah normally wiring power to these does actually power the Arduino, however as I mentioned my issue was that these were occupied. 
    Now that I know these can be soldered I'll give it a try and see if it works, thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Adam_A
    0 Adam_A over 3 years ago in reply to Andrew J

    Here is an actual picture of my board, it says UNO on it

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to Adam_A

    Looks like a clone that has taken advantage of the smaller ATMega SMD version, to provide extra access to the signals and power rails.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Adam_A
    0 Adam_A over 3 years ago in reply to Jan Cumps

    Yeah I plugged in an LED to these and it lit up, however you cannot reverse power through them as far as I  know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 3 years ago in reply to Jan Cumps

    Yes, good point Jan/Dave - I missed that too.  Could I just add that the 5V connection there is the 5V rail used across the UNO and any plugged in boards.  You must be very careful not to over supply to this pin, it should preferably be a regulated 5V supply, and for safety's sake you should not connect power to the USB or Barrel Jack whilst it is powered through that pin.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to Adam_A

    You can power a standard UNO through the 5V, if you don't connect other sources (check UNO Rev3):

    docs.arduino.cc/.../power-pins

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Adam_A
    0 Adam_A over 3 years ago in reply to Andrew J

    I did indeed try and "supply" power through the 12 Hole port thing however this ended up with my Power Supply Auto Shutting off to prevent shorting I guess. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to Adam_A

    Do you have USB plugged in?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 3 years ago in reply to Jan Cumps

    As I said, and it should be regulated.  Also, check what current that board can provide through its 5V port vs the current required by the Uno and display (whichever need is greater.)  It should be ok, but it's worth checking. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 3 years ago in reply to Jan Cumps

    As I said, and it should be regulated.  Also, check what current that board can provide through its 5V port vs the current required by the Uno and display (whichever need is greater.)  It should be ok, but it's worth checking.