Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sleep timer in Adafruit Feather nRF52 Bluefruit LE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 414 subscribers
  • Views 4587 views
  • Users 0 members are here
  • sleep
  • timer
  • interval
  • nrf52
Related

Sleep timer in Adafruit Feather nRF52 Bluefruit LE

KKaushik
KKaushik over 3 years ago
I'm working with Adafruit Feather nRF52 Bluefruit LE here
I'm trying to code this module to sleep and wake with an internal timer automatically with a fixed interval
The code example is given:
/*
  Blink_sleep
  Turns on an LED on for one second, then off for one second, until the time to go to sleep runs out.
  You can wake up the feather by pressing a key/switch connecting the WAKE_LOW_PIN to GND and the WAKE_HIGH_PIN to 3.3V (VCC)

  Based on the blinky arduino example 
  
  This example code is in the public domain.

  created 19 Jan 2010
  by Pierre Constantineau

*/
#include <Arduino.h>
#include <Adafruit_TinyUSB.h> // for Serial
#include <bluefruit.h>

#define WAKE_LOW_PIN  PIN_A0
#define WAKE_HIGH_PIN PIN_A1

#define SLEEPING_DELAY 30000                                // sleep after 30 seconds of blinking

void gotoSleep(unsigned long time)
{
  // shutdown when time reaches SLEEPING_DELAY ms
  if ((time>SLEEPING_DELAY))
  {
    // to reduce power consumption when sleeping, turn off all your LEDs (and other power hungry devices)
    digitalWrite(LED_BUILTIN, LOW);                     

    // setup your wake-up pins.
    pinMode(WAKE_LOW_PIN,  INPUT_PULLUP_SENSE);    // this pin (WAKE_LOW_PIN) is pulled up and wakes up the feather when externally connected to ground.
    pinMode(WAKE_HIGH_PIN, INPUT_PULLDOWN_SENSE);  // this pin (WAKE_HIGH_PIN) is pulled down and wakes up the feather when externally connected to 3.3v.
 
    // power down nrf52.
    sd_power_system_off();                              // this function puts the whole nRF52 to deep sleep (no Bluetooth).  If no sense pins are setup (or other hardware interrupts), the nrf52 will not wake up.
  } 
}

// the setup function runs once when you press reset or power the board
void setup() {
  Bluefruit.begin();          // Sleep functions need the softdevice to be active.

  // initialize digital pin LED_BUILTIN as an output.
  pinMode(LED_BUILTIN, OUTPUT);
}
     
// the loop function runs over and over again forever
void loop() {
  digitalToggle(LED_BUILTIN); // turn the LED on (HIGH is the voltage level)
  gotoSleep(millis());        // call millis() and pass it to the sleep function.  On wake-up, millis will start at 0 again.
  delay(1000);                // wait for a second
}
 
"Turns on an LED on for one second, then off for one second, until the time to go to sleep runs out. You can wake up the feather by pressing a key/switch connecting the WAKE_LOW_PIN to GND and the WAKE_HIGH_PIN to 3.3V (VCC)"
 
I could find only a function "sd_app_evt_wait();" to use instead of "sd_power_system_off();" // this function puts the whole nRF52 to deep sleep (no Bluetooth). If no sense pins are setup (or other hardware interrupts), the nrf52 will not wake up.
I need help configuring the internal timer to wake the module from sleep. But if anyone has worked on it, please help me.
Git Source for Library used in Example Code : here
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2 verified
    There's example code here: https://github.com/NordicPlayground/nrf51-TIMER-examples/blob/master/timer_example_timer_mode/main.c It's not written in Arduino, but you'll get the idea. Basically, the…
Parents
  • shabaz
    +1 shabaz over 3 years ago

    There's example code here:

    https://github.com/NordicPlayground/nrf51-TIMER-examples/blob/master/timer_example_timer_mode/main.c

    It's not written in Arduino, but you'll get the idea. Basically, the timer is set up and the WFE instruction is used to tell the microcontroller to go to sleep until the timer event occurs.

    You'd have to implement that in Arduino using register writes (refer to the microcontroller user manual to figure out how to do that) and assembler instruction. There may be other ways to do it, but the method described would work, since the non-arduino example code does that.

    Please share the arduino code once you have done it, to help others.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    +1 shabaz over 3 years ago

    There's example code here:

    https://github.com/NordicPlayground/nrf51-TIMER-examples/blob/master/timer_example_timer_mode/main.c

    It's not written in Arduino, but you'll get the idea. Basically, the timer is set up and the WFE instruction is used to tell the microcontroller to go to sleep until the timer event occurs.

    You'd have to implement that in Arduino using register writes (refer to the microcontroller user manual to figure out how to do that) and assembler instruction. There may be other ways to do it, but the method described would work, since the non-arduino example code does that.

    Please share the arduino code once you have done it, to help others.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • KKaushik
    0 KKaushik over 3 years ago in reply to shabaz

    I'll update it here if I figured out how to do it.