Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum more Arduino silliness.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 411 subscribers
  • Views 5730 views
  • Users 0 members are here
  • arduino IDE 2.0.3
Related

more Arduino silliness.

phoenixcomm
phoenixcomm over 3 years ago

As a C programmer and learning Java,  I like to keep things VERY SIMPLE!!!

so normally I would have my file pins.h which would include a bunch of #defines like RST_1 13, etc. This now keeps me sane when trying to use it and stops me from wondering if is it this pin or that pin. (for amplification please see it below.  

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

So in the same header file I also want my pinMode statements which now can use my mnemonics rather than the stupid pin number.  this now is hitting close to 20-30 lines. 

#define RST_1 13
#define RST_1 12
pinMode(RST_1, OUTPUT);
pinMode(RST_2, OUTPUT);
BUT THE IDE tosses errors like  error: expected constructor, destructor, or type conversion before '(' token pinMode (RST_1, OUTPUT);

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +4
    Hi Cris, It might be because the first line is defining RST_1, but the second line is defining it a second time, i.e. it states RST_1 on the second line too, where it should be RST_2 I guess. However…
  • baldengineer
    baldengineer over 3 years ago in reply to phoenixcomm +4
    phoenixcomm said: THEREFORE either the definition of pinMode(pin, mode); LIES where pin MUST be a value. which I don't believe THEN AND I DO BELEIVE the #define is not being substituted at compile time…
  • ntewinkel
    ntewinkel over 3 years ago in reply to shabaz +4
    shabaz , that looks great. I like your organized programming style. I totally agree on the readability of the code - it's not often we're stuck with the tiniest of chips anymore, so I too will choose…
Parents
  • shabaz
    shabaz over 3 years ago

    Hi Cris,

    It might be because the first line is defining RST_1, but the second line is defining it a second time, i.e. it states RST_1 on the second line too, where it should be RST_2 I guess.

    However, the error text doesn't help as much as it could.

    Incidentally, some IDEs will detect this as it is typed, and flag it as an error before compilation. With CLion, if I try to do that, I see this:

    image

    It automatically shades the second 'BOB' to indicate an issue. If I hover over it, then it states the reason, sometimes in a better way than a compiler:

    image

    I guess Arduino code could be typed in CLion first, and then copy-pasted into the Arduino IDE, or perhaps it allows a different editor to be used.

    CLion is not free unfortunately though, so this isn't an option always, but just mentioning it in case there are other IDEs with this sort of capability too, that people may be aware of.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to shabaz

    I believe NexGen is trying to find a convient way to set the pinmode in a header file, Im not sure of the answer...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 3 years ago in reply to shabaz

    I believe NexGen is trying to find a convient way to set the pinmode in a header file, Im not sure of the answer...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 3 years ago in reply to scottiebabe

    Right, you can't (or at least shouldn't) be running executable code in a header file.

    So in addition to the RST_1 being defined twice, maybe the goal is to also #define the pinmode() calls to reduce it down?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Oh, I missed that bit of the question. I can't think of better options than what Nico suggests either. Either a nice setup() or init() type of function, or the OO method with each defined class implementing its own initialization code. Technically the latter in C++ allows the code to reside in the header file if that's really desired, but whether that is good practice or not for this scenario, is another issue (personally I would put it in the C file).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to shabaz

    That's what I normally do, though the my setup function ends up being a monster having to deal with input versus output, pullups, analog select, peripheral mapping, interrupts, clocks, etc etc but the Arduino environment takes care of most of that for you. Microchip provides structs with bitwise access for all their peripherals the same could be done on any mcu platform for example

    typedef struct tagPORTABITS {
      uint16_t RA0:1;
      uint16_t RA1:1;
      uint16_t RA2:1;
      uint16_t RA3:1;
      uint16_t RA4:1;
    } PORTABITS;
    extern volatile PORTABITS PORTAbits __attribute__((__sfr__));

    /* PORTA */
    #define _RA0 PORTAbits.RA0
    #define _RA1 PORTAbits.RA1

    So to write to a gpio pin,

    _LATA0 = 1; // of course you can add a custom define for _LATA0...

    If its an input you would read from the port input, if its an output you would write to the output latch