Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Montana Kid's Robotics Club Continuous 2 servo locomotion Is there a way to command the servo to completely stop?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 412 subscribers
  • Views 1395 views
  • Users 0 members are here
Related

Montana Kid's Robotics Club Continuous 2 servo locomotion Is there a way to command the servo to completely stop?

PROFCW
PROFCW over 3 years ago

We are building an IR Arduino uno controlled (from NEC remote)  mobile robot with two servos.  Now we used the usual servo library and it worked well until we tried to stop the servo. The servo will drift ever so slightly, because the servo is updated about every 20 milliseconds, therefore it drifts and the robot at stop continues to move.  Is there a way to command the servo to completely stop?  I thought of a cutoff power rellay but maybe there's a better way

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Both ways are good. If you kill the PWM signal (e.g. reconfigure the pin to be an input or set the PWM to an invalid value) then a decent (or semi-decent, or even some very low-end! but not always) hobby…
  • dougw
    dougw over 3 years ago +1
    Servo hunting or drift may be due to several things like load, servo position, coupling stiffness, local vibration, power fluctuations, etc. Hobby servos typically don't have adjustable loop gain or integral…
  • strb
    strb over 3 years ago +1
    Based on your description I understand that after setting the value that should means "no servo rotation" you continue getting a slight rotation, right? If so, you could try to find by trial and error…
Parents
  • dougw
    dougw over 3 years ago

    Servo hunting or drift may be due to several things like load, servo position, coupling stiffness, local vibration, power fluctuations, etc. Hobby servos typically don't have adjustable loop gain or integral and derivative feedback control so other solutions are needed. Power removal, like you suggest, is one method that would work if the load doesn't cause movement. You could also try just stopping the PWM signal to the servo. Another method is to add a large capacitor to the servo motor power supply right at the servo motor. This reduces power supply fluctuations due to servo activity.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    Servo hunting or drift may be due to several things like load, servo position, coupling stiffness, local vibration, power fluctuations, etc. Hobby servos typically don't have adjustable loop gain or integral and derivative feedback control so other solutions are needed. Power removal, like you suggest, is one method that would work if the load doesn't cause movement. You could also try just stopping the PWM signal to the servo. Another method is to add a large capacitor to the servo motor power supply right at the servo motor. This reduces power supply fluctuations due to servo activity.