Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Logic for flame sensor which is mounted on 4 DOF robotic arm ,so when flame gets detected it should lock /follow the flame
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 413 subscribers
  • Views 15344 views
  • Users 0 members are here
  • mega
  • embedded c
  • robotics
  • robot
  • projects
  • programming
  • arduino_code
  • code
  • adafruit
  • sensor
Related

Logic for flame sensor which is mounted on 4 DOF robotic arm ,so when flame gets detected it should lock /follow the flame

headhoe_15
headhoe_15 over 3 years ago

note : 5 channel flame sensor is used which is mounted on the end effector of the arm,and the robotic arm scan does 180 degree scanning...So experts you are all in here..
a image of code has been attached here so feel free to correct the code. hey listen m also using PCA9685 Servo motor driver to control the robotic arm ,,,i just only need the help in following / tracking of the flame once its get detected ??????

#include <Wire.h>
#include <Adafruit_PWMServoDriver.h>

#define FLAME_SENSOR_PIN A0
#define FIRE_THRESHOLD 200
#define MIN_ANGLE 0
#define MAX_ANGLE 180

Adafruit_PWMServoDriver pwm = Adafruit_PWMServoDriver();
int servoPin = 0;

void setup() {
  Serial.begin(9600);
  pwm.begin();
  pwm.setPWMFreq(60);
}

void loop() {
  for (int angle = MIN_ANGLE; angle <= MAX_ANGLE; angle++) {
    pwm.setPWM(servoPin, 0, map(angle, 0, 180, 120, 620));
    int flameValue = analogRead(FLAME_SENSOR_PIN);
    if (flameValue > FIRE_THRESHOLD) {
      Serial.println("Fire detected!");
      break;
    }
    delay(20);
  }
}

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Regarding " i just only need the help in following / tracking of the flame once its get detected " isn't that the main, core part of the project? Your code lines 20-25 already implement your algorithm…
  • beacon_dave
    beacon_dave over 3 years ago +3
    Perhaps if you were to read the other 4 sensor channels as well, then you can detect the flame moving to the left or to the right and then move your robot arm in the same direction until it is back in…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +2
    Probably some college project! I remember doing a course for a few months at some college in the middle of nowhere (Bracknell) where they wanted you to track a microwave source, i.e. exactly the same thing…
  • shabaz
    shabaz over 3 years ago

    Regarding "i just only need the help in following / tracking of the flame once its get detected"

    isn't that the main, core part of the project? 

    Your code lines 20-25 already implement your algorithm* to identify the direction. If you want to move some device to orient itself into that direction, look up something called 'inverse kinematics'. It involves you coming up with a model (formula) that can take the angle (from your line 20) and translate that into the angle that your robot arm needs to move, in a number of motion axes (depends on your robot arm). You can do some of it with a pen and paper, drawing the mechanism of your arm, and then using trigonometry. And then implementing that inside your code. Note: It won't necessarily be easy. If this is a school project then get someone good at trigonometry to help you. It's high-school level of maths, so not overly difficult, but requires someone to put some effort in.

    *That algorithm could be improved too. It's up to you how sophisticated you make it. You'll soon discover how you may wish to improve it, if you use (say) the Arduino plotting tool to see sensor values in real life, with a flame or other heat source.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • headhoe_15
    headhoe_15 over 3 years ago in reply to shabaz

    hey listen , can you suggest a more detail on how to code the flame tracking movement of  robotic arm when the fire is detected through the 5 channel flame sensor ...?????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago

    Perhaps if you were to read the other 4 sensor channels as well, then you can detect the flame moving to the left or to the right and then move your robot arm in the same direction until it is back in the centre again. If you lose it, then do a full sweep until you find it again.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • headhoe_15
    headhoe_15 over 3 years ago in reply to beacon_dave

    I am using following components in the my project :

    1. 12 v dc motor for vehicle movement
    2. Ultrasonic sensor for obstacle avoidance.
    3. 4 DOF robotic arm
    4. 5 -channel flame sensor
    5. 12 v submersible pump
    6. Arduino mega 2560 microcontroller.
      Problem : After detecting fire through flame sensor.robotic arm position is not getting freezed but its coming to the initial position.
      once the fire is detected through flame sensor ,robotic arm should move forward to the flame,the position of the arm should be freezed and vehicle should move towards the fire, a water should be sprayed on the fire ,once the fire is extinguished a arm should again scan for any remaining fire by scanning from 0 to 180 degree for three different levels of height, if its detect another fire same position of the arm should be repeated ,and when all fire are extinguish ,the arm should come to its initial position.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to headhoe_15

    "5 -channel flame sensor" - means that there are 5 sensors available (approx 30 degrees each) but the code shown is only reading one of the 5 analogue sensor outputs. If you read all 5 channels, then you will likely get a better indication of the position of a single flame.

    "position is not getting freezed but its coming to the initial position" - the Arduino loop() function runs continually, so your for loop is called continually and each time the for loop runs it sets angle back to MIN_ANGLE. 

    --

    This looks like a cross-posting

    https://forum.allaboutcircuits.com/threads/logic-for-flame-sensor-which-is-mounted-on-4-dof-robotic-arm-so-when-flame-gets-detected-it-should-lock-follow-the-flame.191992/

    https://forum.arduino.cc/t/logic-for-flame-sensor-which-is-mounted-on-4-dof-robotic-arm-so-when-flame-gets-detected-it-should-lock-follow-the-flame/1090192

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave

    Probably some college project! I remember doing a course for a few months at some college in the middle of nowhere (Bracknell) where they wanted you to track a microwave source, i.e. exactly the same thing except swap out the flame sensor for any desired number of 'detector diodes' plus whatever op-amp amplifier we could come up with. I can't recall what microcontroller we used. Instead of servo motors we used stepper motors, sitting in a gimbal-like mechanism that was quite a challenge to design/construct. It is a lot easier these days with ready-made robot arms etc.