Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Looking for a small display recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 413 subscribers
  • Views 6664 views
  • Users 0 members are here
  • displays
  • model railroad
  • arduino projects
Related

Looking for a small display recommendation

colporteur
colporteur over 3 years ago

Does any member have a recommendation for a small display that is appropriate for scrolling from right to left?

After an hour culling the adafruit website with few returns, I have come to the E14 community hopefully to get a recommendation. I've been asked to build a two signs, one that scrolls "Welcome to Snow Island"  and the other "Thank you for Visiting Snow" Island. The signs will be positioned on top of a bridge on an HO scale model railroad layout.

I had hoped to use a MAX7219 Dot led Matrix MCU 8x32 but it is way to large for the foot print I have to work with. The bridge has a large flat surface about 4X4 inches to hold the sign.

Like any model railroad project cost is a factor. I don't have a big budget. I'm hoping to combine the display with an Nano Arduino to simulate a continuous text scrolling road sign to message visitors.

If your suggestions could contain the source for the part that would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +5
    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right…
  • colporteur
    colporteur over 3 years ago in reply to colporteur +4
    community.element14.com/.../IMG_5F00_2289.MOV Do I buy or do I build? The S1144 (far left) displays arrived today. After installing the configuration software the display I wanted was working. At $10…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Just saw these, look quite nice, just under 3.7" wide, available in many colors, and very cheap! However they either work for the use-case, or don't, since the behaviour of them is only configurable…
Parents
  • robogary
    robogary over 3 years ago

    4 X 4 is a tough nut to crack for alphanumerics, the aspect ratio doesnt fit the usual. Could a 1602 LCD do the job ?  https://www.amazon.com/NOYITO-Yellow-Green-Backlight-Interface-MEGA2560/dp/B07SZV1MK8/ref=sr_1_13?crid=73DPEGA7PT9Q&keywords=lcd+1602+module&qid=1677080223&sprefix=lcd+1602%2Caps%2C151&sr=8-13

     https://www.amazon.com/Qunqi-Serial-Backlight-Arduino-MEGA2560/dp/B01E4YUT3K/ref=sr_1_11?crid=2DZB5X1BBJQTT&keywords=iic+%2F+i2c+1602+blue+backlight+lcd+display+screen+module&qid=1677080327&sprefix=lcd+1602+module%2Caps%2C287&sr=8-11

    SSD1306 displays work well, but they are 1.3 inches square at best. There are some bigger TFT screens, but I hadnt worked with them to say how easy they are, and of course they start to get pricey as the size increases. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago

    4 X 4 is a tough nut to crack for alphanumerics, the aspect ratio doesnt fit the usual. Could a 1602 LCD do the job ?  https://www.amazon.com/NOYITO-Yellow-Green-Backlight-Interface-MEGA2560/dp/B07SZV1MK8/ref=sr_1_13?crid=73DPEGA7PT9Q&keywords=lcd+1602+module&qid=1677080223&sprefix=lcd+1602%2Caps%2C151&sr=8-13

     https://www.amazon.com/Qunqi-Serial-Backlight-Arduino-MEGA2560/dp/B01E4YUT3K/ref=sr_1_11?crid=2DZB5X1BBJQTT&keywords=iic+%2F+i2c+1602+blue+backlight+lcd+display+screen+module&qid=1677080327&sprefix=lcd+1602+module%2Caps%2C287&sr=8-11

    SSD1306 displays work well, but they are 1.3 inches square at best. There are some bigger TFT screens, but I hadnt worked with them to say how easy they are, and of course they start to get pricey as the size increases.