Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Quiz button
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 414 subscribers
  • Views 1285 views
  • Users 0 members are here
Related

Quiz button

FADHLAN2008
FADHLAN2008 over 3 years ago

Hello everyone. Please help...
#include "DFRobotDFPlayerMini.h"
#include "SoftwareSerial.h"

// Use pins 2 and 3 to communicate with DFPlayer Mini
static const uint8_t PIN_MP3_TX = 2; // connect to pin 2 on the DFPlayer via a 1K resistor
static const uint8_t PIN_MP3_RX = 3; // connect to pin 3 on the DFPlayer

// Software serial library
SoftwareSerial softwareSerial(PIN_MP3_RX, PIN_MP3_TX);
// Player
DFRobotDFPlayerMini player;

// Pins for buttons
const unsigned char switches[4] = {A7, A6, A5, A4};

// Pins for LEDs
const unsigned char leds[4] = {4, 5, 6, 7};

// Reset button
const unsigned char switch_reset = A2;

// Prepare the Arduino
void setup() {
// Prepare the pins

pinMode(switch_reset, INPUT_PULLUP);
for (unsigned char sw=0; sw<4; sw++) {
pinMode(switches[sw], INPUT_PULLUP);
pinMode(leds[sw], OUTPUT);
digitalWrite(leds[sw], LOW);
}

// Init serial port for DFPlayer Mini
softwareSerial.begin(9600);
// Start communication with DFPlayer Mini
if (player.begin(softwareSerial)) player.volume(30);
player.play(11);
while (digitalRead(switch_reset) == HIGH) {};
// Stop any playing sfx
player.stop();
}

// Main loop
void loop() {
// Check all 4 switches
for (unsigned char sw=0; sw<4; sw++) {
// Is it pressed?
if (digitalRead(switches[sw]) == LOW) {
// Turn on its LED
digitalWrite(leds[sw], HIGH);
// Play its sfx
player.play(sw+1);
// Wait for the reset button
while (digitalRead(switch_reset) == HIGH) {};
// Stop any playing sfx
player.stop();
// Turn off the LED
digitalWrite(leds[sw], LOW);
// Stop!
break;
}
}
}

how to add button right and button wrong answer before reset after arduino pins A4-A7 are pressed

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +1
    Please insert code using the Insert -> Code option, as otherwise your code is mangled and difficult to read. You will need to explain exactly what it needs to do, how it works at the moment and what…
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    Please insert code using the Insert -> Code option, as otherwise your code is mangled and difficult to read.

    You will need to explain exactly what it needs to do, how it works at the moment and what is wrong for us to have any chance of helping you. Also, explain what equipment you are using - what is the board and the peripherals you are using?

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago

    Please insert code using the Insert -> Code option, as otherwise your code is mangled and difficult to read.

    You will need to explain exactly what it needs to do, how it works at the moment and what is wrong for us to have any chance of helping you. Also, explain what equipment you are using - what is the board and the peripherals you are using?

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to Gough Lui

    Looks like it is connecting to a DFRobot DFPlayer mini MP3 player module:
    https://www.dfrobot.com/product-1121.html

    Presumably trying to add an extra couple of button inputs to the existing four track select/play buttons and the one stop/reset button to alter playback in some way for a music quiz.

    The same question has been cross posted to the Arduino forum
    https://forum.arduino.cc/t/competition-button/1092250