Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino UNO R4 coming shortly
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 413 subscribers
  • Views 5145 views
  • Users 0 members are here
  • uno
  • arduino
Related

Arduino UNO R4 coming shortly

Andrew J
Andrew J over 3 years ago

Saw this today: Arduino UNO r4 on the official site.

Renesas processor, 32-bit, 256MB ram CAN bus and more.  Should really open up new projects and give the Mega a run for its money.  Actually makes you wonder what they might do with that one now.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +7
    Neat. What's also great to see is they are continuing to invest in the arduino library catalog
  • Gough Lui
    Gough Lui over 3 years ago +3
    Hmm. An interesting development indeed. Still 5V, but the loss of AVR doesn't feel like Uno to me ... But perhaps a good move overall ... I wonder how it stacks up to the SAMD-family that has been running…
  • shabaz
    shabaz over 3 years ago +3
    Looks good! I might actually want to finally use an Uno! However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic. Granted lots…
Parents
  • shabaz
    shabaz over 3 years ago

    Looks good! I might actually want to finally use an Uno!

    However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic.

    Granted lots of industrial interface chips still use 5V, but it would be nice to also support 3.3V in some way for at least a few GPIO, e.g. a few level converters on-board. Still, looks like I2C will work at 3.3V according to the table below (unless Arduino has I2C resistors on-board, I don't know if Arduino boards do that or not; anyway it's not hard to desolder them, lets hope they are not 0201 silliness, if this is an industrial-targeted board).

    image

    One great thing with Renesas is the always almost OTT level of documentation, it's a 1400-page extremely detailed reference manual : ) 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz

    I assume one of the things they strove for was backwards compatibility with all the shields out there, as well as existing projects.   For a lot of people, the biggest "win" will be the memory increases opening up a lot more extended feature possibilities.  It would have been useful to provide a 3.3V option though.  The R3 Uno definitely didn't have on-board I2C resistors.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz

    I assume one of the things they strove for was backwards compatibility with all the shields out there, as well as existing projects.   For a lot of people, the biggest "win" will be the memory increases opening up a lot more extended feature possibilities.  It would have been useful to provide a 3.3V option though.  The R3 Uno definitely didn't have on-board I2C resistors.