Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino UNO R4 coming shortly
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 413 subscribers
  • Views 5133 views
  • Users 0 members are here
  • uno
  • arduino
Related

Arduino UNO R4 coming shortly

Andrew J
Andrew J over 3 years ago

Saw this today: Arduino UNO r4 on the official site.

Renesas processor, 32-bit, 256MB ram CAN bus and more.  Should really open up new projects and give the Mega a run for its money.  Actually makes you wonder what they might do with that one now.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +7
    Neat. What's also great to see is they are continuing to invest in the arduino library catalog
  • Gough Lui
    Gough Lui over 3 years ago +3
    Hmm. An interesting development indeed. Still 5V, but the loss of AVR doesn't feel like Uno to me ... But perhaps a good move overall ... I wonder how it stacks up to the SAMD-family that has been running…
  • shabaz
    shabaz over 3 years ago +3
    Looks good! I might actually want to finally use an Uno! However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic. Granted lots…
Parents
  • shabaz
    shabaz over 3 years ago

    Looks good! I might actually want to finally use an Uno!

    However this could be a bit of a pain, unless VCC can be changed to 3.3V, otherwise level shifters will be needed with 3.3V logic.

    Granted lots of industrial interface chips still use 5V, but it would be nice to also support 3.3V in some way for at least a few GPIO, e.g. a few level converters on-board. Still, looks like I2C will work at 3.3V according to the table below (unless Arduino has I2C resistors on-board, I don't know if Arduino boards do that or not; anyway it's not hard to desolder them, lets hope they are not 0201 silliness, if this is an industrial-targeted board).

    image

    One great thing with Renesas is the always almost OTT level of documentation, it's a 1400-page extremely detailed reference manual : ) 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago in reply to shabaz

    You've got me trawling through the Renesas RA4M1 spec now...

    Spotted this... I will be curious to see how the Arduino R4 handles all these analogue capabilities the chipset offers:

    • has both a 14-bit A/D Converter (ADC14) and a 12-bit D/A Converter (DAC12)
    • has 2 x 8-bit D/A Converters (DAC8)
    • has 2 x Low-Power Analog Comparators
    • and 4 x Operational Amplifiers
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 3 years ago in reply to shabaz

    You've got me trawling through the Renesas RA4M1 spec now...

    Spotted this... I will be curious to see how the Arduino R4 handles all these analogue capabilities the chipset offers:

    • has both a 14-bit A/D Converter (ADC14) and a 12-bit D/A Converter (DAC12)
    • has 2 x 8-bit D/A Converters (DAC8)
    • has 2 x Low-Power Analog Comparators
    • and 4 x Operational Amplifiers
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 3 years ago in reply to BigG

    Hmm. Well the analogReadResolution() call already exists, and did hint at choosing higher values for some "forward compatibility". LSBs will be padded with zeroes where the hardware is not capable of the requested resolution.

    I guess analogWrite() can be real analog rather than PWM now too ...

    As for the others ... I suppose they'll roll out the new functions assuming they're available and hooked up. Or else, like some more advanced features, people will have to access ports directly and twiddle bits to get the desired outcomes.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Gough Lui

    It would probably be a pleasure using that chip with direct register access, with the detailed documentation with plentiful diagrams etc throughout. Actually, since the part is available in easy-to-solder packages too (QFP and there's a 0.5 mm pitch QFN option too), it would also be often convenient to just directly use the chip without the Uno. Just saw there's a reasonable-price RA4M1 dev-board for one of the 100-pin QFP variants. I'm thinking it could be worth getting that, just to try out the device. It would be nice to try the analog functionality that BigG spotted.

    Also it's a nice part for upgradeability in the field, since it has serial and USB bootloader.