Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When to use int, const int, const byte and Define
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 411 subscribers
  • Views 14797 views
  • Users 0 members are here
  • programming
  • arduino_code
  • development
Related

When to use int, const int, const byte and Define

colporteur
colporteur over 3 years ago

I'm not a programmer. I am more of a ressurectionist. I find Arduino code pieces and join them together to make a program like Dr. Frankenstein joined body parts to create his monster. 

I see the statements listed in the question and wondered when do they apply. In collecting code parts from a number of programs, I can develop a program that has all four before the voids.  If I was to create a program from scratch I'm not confident I know what one to select for the variable type I am using.

Are there some best practices a novice could use in applying these to get the most benefit from their programming?

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    Personally, I used to only use #define for text-replacement. So, things like #define NOT_PRESSED 0x1, and #define PRESSED 0x0 for buttons. It makes if-statements more readable. For example, (if digitalRead…
  • Andrew J
    Andrew J over 3 years ago +4
    colporteur said: Are there some best practices a novice could use in applying these to get the most benefit from their programming? Please take this the right way: the best thing you could do is sit…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Foo and bar are the worst! It never made sense. Reminded me of the stereotype of the nerd who deliberately uses the most complex sed/awk syntax he/she can think of. Especially since it doesn't take a genius…
Parents
  • baldengineer
    baldengineer over 3 years ago

    Personally, I used to only use #define for text-replacement. So, things like #define NOT_PRESSED 0x1, and #define PRESSED 0x0 for buttons. It makes if-statements more readable. For example, (if digitalRead(pin) == NOT_PRESSED.) Good solution for people who mistakenly think that pull-ups make the inputs inverted.

    In the past, I would always define things like pin functions as a const. But lately, I've been using #defines more. For any value that will fit into an 8-bit number, there is no performance difference between a #define macro or a const (of an 8-bit variable type.) For a const that fits into a register, most compilers won't bother treating it as a variable anyway.

    As usual, it is more important to be consistent in your code than get worked up over which is better.

    Regarding int versus byte, versus, whatever, except for byte and char, I have stopped using types like int. Instead, I use fixed-width integer types like uint8_t or uint32_t or int8_t. These are all part of stdint.h.

    Using fixed width removes the ambiguity of "How big is this variable on this processor with this compiler on this week of the year?"

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to baldengineer

    Definitely the fixed width types, otherwise I find myself in the situation JWx mentions: at least .... and off we go to the races to find out what size is actually is.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to baldengineer

    Definitely the fixed width types, otherwise I find myself in the situation JWx mentions: at least .... and off we go to the races to find out what size is actually is.