Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When to use int, const int, const byte and Define
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 411 subscribers
  • Views 14761 views
  • Users 0 members are here
  • programming
  • arduino_code
  • development
Related

When to use int, const int, const byte and Define

colporteur
colporteur over 3 years ago

I'm not a programmer. I am more of a ressurectionist. I find Arduino code pieces and join them together to make a program like Dr. Frankenstein joined body parts to create his monster. 

I see the statements listed in the question and wondered when do they apply. In collecting code parts from a number of programs, I can develop a program that has all four before the voids.  If I was to create a program from scratch I'm not confident I know what one to select for the variable type I am using.

Are there some best practices a novice could use in applying these to get the most benefit from their programming?

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    Personally, I used to only use #define for text-replacement. So, things like #define NOT_PRESSED 0x1, and #define PRESSED 0x0 for buttons. It makes if-statements more readable. For example, (if digitalRead…
  • Andrew J
    Andrew J over 3 years ago +4
    colporteur said: Are there some best practices a novice could use in applying these to get the most benefit from their programming? Please take this the right way: the best thing you could do is sit…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Foo and bar are the worst! It never made sense. Reminded me of the stereotype of the nerd who deliberately uses the most complex sed/awk syntax he/she can think of. Especially since it doesn't take a genius…
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    OMG  "colporteur "When to use int, const int, const byte and Define", I have been working with K&R and then ANSI C since the mid '70s.  Let me start at the top and work to the bottom;

    • int ::= any time you want any sort of number (whole only)
    • cont int        this is stupid lets me tell the compiler that I am not going to change its value; 
    • const byte   "
    • #define::=  This is a macro;  I use this to assign values for a named variable such as "#define FAIL -1;" or things that are not in the library like the value of pi. or a square "#define sqr(a)  ((a)*(a)",  

    NOTE: error messages and I have quite a few some of my boxes will have 50+ error messages. here is the best way to handle them. The key is to standardize them. so lets build a structure of error messages:

    typedef struct eMessages{
      int errorNumber;
      int equipment; 
      int formatType;     // this is info we send to the formatter
      char[200] error;    //message long
      char[20]  errorsh;  //short version
      } errorMessages;
      
      all error messages can now be unified
      
      void ErrorMessage(int errorNumber, int equipment, int formatType ){
      time_t current_raw_time = time(0); // System time:
       printf ( "%02d:%02d:%02d: #%10d -- #%u -- %s200 \n" errorMessages, int equipment, formatType);

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago

    OMG  "colporteur "When to use int, const int, const byte and Define", I have been working with K&R and then ANSI C since the mid '70s.  Let me start at the top and work to the bottom;

    • int ::= any time you want any sort of number (whole only)
    • cont int        this is stupid lets me tell the compiler that I am not going to change its value; 
    • const byte   "
    • #define::=  This is a macro;  I use this to assign values for a named variable such as "#define FAIL -1;" or things that are not in the library like the value of pi. or a square "#define sqr(a)  ((a)*(a)",  

    NOTE: error messages and I have quite a few some of my boxes will have 50+ error messages. here is the best way to handle them. The key is to standardize them. so lets build a structure of error messages:

    typedef struct eMessages{
      int errorNumber;
      int equipment; 
      int formatType;     // this is info we send to the formatter
      char[200] error;    //message long
      char[20]  errorsh;  //short version
      } errorMessages;
      
      all error messages can now be unified
      
      void ErrorMessage(int errorNumber, int equipment, int formatType ){
      time_t current_raw_time = time(0); // System time:
       printf ( "%02d:%02d:%02d: #%10d -- #%u -- %s200 \n" errorMessages, int equipment, formatType);