Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When to use int, const int, const byte and Define
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 411 subscribers
  • Views 14747 views
  • Users 0 members are here
  • programming
  • arduino_code
  • development
Related

When to use int, const int, const byte and Define

colporteur
colporteur over 3 years ago

I'm not a programmer. I am more of a ressurectionist. I find Arduino code pieces and join them together to make a program like Dr. Frankenstein joined body parts to create his monster. 

I see the statements listed in the question and wondered when do they apply. In collecting code parts from a number of programs, I can develop a program that has all four before the voids.  If I was to create a program from scratch I'm not confident I know what one to select for the variable type I am using.

Are there some best practices a novice could use in applying these to get the most benefit from their programming?

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    Personally, I used to only use #define for text-replacement. So, things like #define NOT_PRESSED 0x1, and #define PRESSED 0x0 for buttons. It makes if-statements more readable. For example, (if digitalRead…
  • Andrew J
    Andrew J over 3 years ago +4
    colporteur said: Are there some best practices a novice could use in applying these to get the most benefit from their programming? Please take this the right way: the best thing you could do is sit…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Foo and bar are the worst! It never made sense. Reminded me of the stereotype of the nerd who deliberately uses the most complex sed/awk syntax he/she can think of. Especially since it doesn't take a genius…
Parents
  • Prasanth_R
    Prasanth_R over 3 years ago

    byte is used primarily in serial communications such as UART, RS485 (Better approach would be using uint8_t for serial communications).
    int is used to hold values from −32,768 to 32,767 which ideal for scenario where 2byte of signed data needs to be stored.
    const int is used as a reference for commonly known value. Such as const int boiling_point = 100 (better approach would be #define BOILING_POINT 100).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to Prasanth_R

    I like the suggestion but I have yet to find examples where it applies. That doesn't mean it is wrong, I have just seen it used to define pins that are not communication related. 

    Now that I have this knowledge I will look for it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Prasanth_R
    Prasanth_R over 3 years ago in reply to colporteur

    Ok, I got your confusion. I created a simple function that prints pin number specified in different data types using Compiler Explorer (godbolt.org)
    As you can see from the assembly language, compiler considers
    #define and const declaration as same and directly copy the absolute value to register.
    int as a 32bit value (double word).
    byte as 8bit value, which compiler copies to lower byte and set 0 to rest of the higher order bytes.

    Considering pin number won't change during compilation or run time and less amount of processing required pin definition can be made using const or #define types.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Prasanth_R
    Prasanth_R over 3 years ago in reply to colporteur

    Ok, I got your confusion. I created a simple function that prints pin number specified in different data types using Compiler Explorer (godbolt.org)
    As you can see from the assembly language, compiler considers
    #define and const declaration as same and directly copy the absolute value to register.
    int as a 32bit value (double word).
    byte as 8bit value, which compiler copies to lower byte and set 0 to rest of the higher order bytes.

    Considering pin number won't change during compilation or run time and less amount of processing required pin definition can be made using const or #define types.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 3 years ago in reply to Prasanth_R

    Thank you for the response. This makes sense to me.

    Best Practice (i.e. it has some advantages), get in the habit of using const or #define when identifying the pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Prasanth_R

    I mess about with this thing. Its fast for running a test. but to get to work please use Eclipse with the GCC toolchain You'll, thank me. 

    I have several of them one for C, one for Java and I have all of the embedded tools on a third. BTW I despise the Arduino IDE, (all I use is setup(), and then I write my own main() which Loop calls!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to phoenixcomm

    I agree with you on Eclipse, GCC.

    When we switch to the Arduino IDE, Setup(), Loop() and your code, I believe that the Arduino approach is better than what you are doing.