Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 412 subscribers
  • Views 2336 views
  • Users 0 members are here
  • lcd
  • libraries
  • dht11
  • arduino
Related

Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.

e14 Contributor
e14 Contributor over 3 years ago

I am not supposed to use any external libraries for any of the components and the libraries used should be user generated/defined. So far i can only display the temp and humidity using downloaded/external libraries: 

#include "LiquidCrystal.h"
LiquidCrystal lcd(8,7,6,5,4,3);
int sensorPin = 0;

void setup()
{
Serial.begin(9600);
lcd.begin(16,2);
}

void loop()
{

int reading = analogRead(sensorPin);

// measure the 5v with a meter for an accurate value
//In particular if your Arduino is USB powered

float voltage = reading * 4.68;
voltage /= 1024.0;

// now print out the temperature

float temperatureC = (voltage - 0.5) * 100;
Serial.print(temperatureC);
Serial.println(" degrees C");

lcd.setCursor(0,0);
lcd.print("Temperature Value ");
lcd.setCursor(0,1);
lcd.print(" degrees C");
lcd.setCursor(11,1);
lcd.print(temperatureC);

delay(100);
}

Please help. Thanks!

  • Sign in to reply
  • Cancel
Parents
  • bidrohini
    0 bidrohini over 3 years ago

    If you are not allowed to use the DHT11.h library, you have to manually do whatever is done by the library. DHT11 uses one wire protocol. You will need OneWire.h

    docs.arduino.cc/.../one-wire

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bidrohini
    0 bidrohini over 3 years ago

    If you are not allowed to use the DHT11.h library, you have to manually do whatever is done by the library. DHT11 uses one wire protocol. You will need OneWire.h

    docs.arduino.cc/.../one-wire

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 3 years ago in reply to bidrohini

    Thank you. I also shouldn't use the liquid crystal library.