Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 412 subscribers
  • Views 2336 views
  • Users 0 members are here
  • lcd
  • libraries
  • dht11
  • arduino
Related

Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.

e14 Contributor
e14 Contributor over 3 years ago

I am not supposed to use any external libraries for any of the components and the libraries used should be user generated/defined. So far i can only display the temp and humidity using downloaded/external libraries: 

#include "LiquidCrystal.h"
LiquidCrystal lcd(8,7,6,5,4,3);
int sensorPin = 0;

void setup()
{
Serial.begin(9600);
lcd.begin(16,2);
}

void loop()
{

int reading = analogRead(sensorPin);

// measure the 5v with a meter for an accurate value
//In particular if your Arduino is USB powered

float voltage = reading * 4.68;
voltage /= 1024.0;

// now print out the temperature

float temperatureC = (voltage - 0.5) * 100;
Serial.print(temperatureC);
Serial.println(" degrees C");

lcd.setCursor(0,0);
lcd.print("Temperature Value ");
lcd.setCursor(0,1);
lcd.print(" degrees C");
lcd.setCursor(11,1);
lcd.print(temperatureC);

delay(100);
}

Please help. Thanks!

  • Sign in to reply
  • Cancel
Parents
  • javagoza
    0 javagoza over 3 years ago

    DHT11 uses a single wire digital communication and you are using the DHT11 as an analog sensor but you have to use a digital input. One communication process is about 4ms. Data consists of decimal and integral parts. A complete data transmission is 40 bit, and the sensor sends higher data bit first.

    Data format: 8 bit integral RH data + 8 bit decimal RH data + 8 bit integral T data + 8 bit decimal T data + 8 bit checksum.

    If the data transmission is right, the checksum should be the last 8bit of: 8 bit integral RH data + 8 bit decimal RH data + 8 bit integral T data + 8 bit decimal T data

    Some years ago I made this post explaining how to read data from the DHT11 DHT11 Arduino Library and ThingSpeak - Hackster.io

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 3 years ago in reply to javagoza

    Thank you! I'll check it out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 3 years ago in reply to javagoza

    Thank you! I'll check it out.