Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 412 subscribers
  • Views 2334 views
  • Users 0 members are here
  • lcd
  • libraries
  • dht11
  • arduino
Related

Using the DHT11 temp and humidity sensor to measure and display the temp and humidity on an LCD screen, without using extrenal libraries.

e14 Contributor
e14 Contributor over 3 years ago

I am not supposed to use any external libraries for any of the components and the libraries used should be user generated/defined. So far i can only display the temp and humidity using downloaded/external libraries: 

#include "LiquidCrystal.h"
LiquidCrystal lcd(8,7,6,5,4,3);
int sensorPin = 0;

void setup()
{
Serial.begin(9600);
lcd.begin(16,2);
}

void loop()
{

int reading = analogRead(sensorPin);

// measure the 5v with a meter for an accurate value
//In particular if your Arduino is USB powered

float voltage = reading * 4.68;
voltage /= 1024.0;

// now print out the temperature

float temperatureC = (voltage - 0.5) * 100;
Serial.print(temperatureC);
Serial.println(" degrees C");

lcd.setCursor(0,0);
lcd.print("Temperature Value ");
lcd.setCursor(0,1);
lcd.print(" degrees C");
lcd.setCursor(11,1);
lcd.print(temperatureC);

delay(100);
}

Please help. Thanks!

  • Sign in to reply
  • Cancel
Parents
  • beacon_dave
    0 beacon_dave over 3 years ago

    There is some info on creating a DHT11 library available here:

    https://link.springer.com/chapter/10.1007/978-1-4302-6838-3_4

    which may be of interest (skip to the end of the chapter.)

    It was written for an Intel Galileo MCU but may be useful if you want examples of the protocol timing in order to roll your own.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 3 years ago in reply to beacon_dave

    Thank you! Will have a look.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 3 years ago in reply to beacon_dave

    Thank you! Will have a look.