Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Why does my Arduino switch Debounce routine bounce?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 411 subscribers
  • Views 6368 views
  • Users 0 members are here
  • arduino_code
  • arduino coding
  • arduino
Related

Why does my Arduino switch Debounce routine bounce?

colporteur
colporteur over 3 years ago

Why does the LED flash twice with one push and release of the button?

#include <Servo.h>

Servo Stop_servo;  // create servo object to control a servo

// Buttons with Pull-Ups are "backwards"
// Some DEFINEs to make reading code easier
#define PUSHED false
#define NOT_PUSHED true
#define WATCH_BUTTON true
#define IGNORE_BUTTON false

// Time to wait for bounce, in MICROsconds
const int buttonWaitInterval = 6000;
// Pins for LED and Button
const int LEDpin = 5;
const int BUTTONpin = 2;
float Minpos = 0;    // variable to store the servo position
float Maxpos = 255;  //greatest travel of servo

// Used to track how long between "bounces"
unsigned long previousMicros = 0;

// Used to track state of button (high or low)
boolean previousButtonState = NOT_PUSHED;

// Variable reporting de-bounced state.
boolean debouncedButtonState = NOT_PUSHED;

// Tracks if we are waiting for a "bounce" event
boolean bounceState = false;

// Nothing surprising here
void setup() {
  pinMode(LEDpin, OUTPUT);
  pinMode(BUTTONpin, INPUT_PULLUP);
  digitalWrite(LEDpin, LOW);
  Stop_servo.attach(3);  // attaches the servo on pin 3 to the servo object
  Stop_servo.write(0);

  Serial.begin(9600);
  Serial.println(F("Serial Initialized"));
}

void loop() {

  // This needs to be called periodically to
  // update the timers and button status
  updateButton();
  // This replaces: digitalRead(BUTTONpin);
  //digitalWrite(LEDpin, debouncedButtonState);
  if (debouncedButtonState == LOW) {
    digitalWrite(LEDpin, HIGH);
    delay(500);
    digitalWrite(LEDpin, LOW);
    delay(500);
    Stop_servo.write(255);
    delay(5000);
    Stop_servo.write(0);
    Serial.println(F("servo cycled"));
  }
}

// All of the magic happens here
void updateButton() {
  // We are waiting for any activity on the button
  if (bounceState == WATCH_BUTTON) {
    // Get and store current button state
    boolean currentButtonState = digitalRead(BUTTONpin);
    // Check to see if a transition has occured (and only one)
    if (previousButtonState != currentButtonState) {
      // A transition was detected, ignore the others for a while
      bounceState = IGNORE_BUTTON;
      // Store current time (start the clock)
      previousMicros = micros();
    }
    // Keep storing existing button state, if we're watching
    previousButtonState = currentButtonState;
  }
  // We are waiting for the buttonWaitInterval to elapse
  if (bounceState == IGNORE_BUTTON) {
    // Compare current value of micros to previously stored, enough time yet?
    unsigned long currentMicros = micros();
    if ((unsigned long)(currentMicros - previousMicros) >= buttonWaitInterval) {
      // Store the state of the button/pin to debouncedButtonState, which "reports"
      // the correct value. This allows for the code to handle active high or low inputs
      debouncedButtonState = digitalRead(BUTTONpin);
      // Go back to watching the button again.
      bounceState = WATCH_BUTTON;
    }
  }
}

I'm trying to use Baldengineer debounce code to read a button and take an action. Each press of the button causes the LED to flash twice. The serial output reflects the routine running twice. 

I have failed in my code changes to get the result I hope. I have looked at Internet and have found no hints to help.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to scottiebabe +4
    Technical forums are great, so many great tidbits of knowledge shared in this thread! One more demonstration showing why a schmitt trigger is an important part of the solution. I wrote a simple PIO…
  • dougw
    dougw over 3 years ago +3
    Debouncing may be good practice, but it would seem you don't need it here. If you start your LED and servo cycle as soon as a button push is first detected, all button bouncing will be long over before…
  • shabaz
    shabaz over 3 years ago +3
    Hi Sean, I've not looked in detail, but it seems that you wish to move a servo just once, if a button is pressed. Your delay() functions are actually already performing a button-pushed-down debounce…
Parents
  • shabaz
    shabaz over 3 years ago

    It's not an entirely "debounce" problem. Debounce is just part of it. That's why you're seeing so many possible approaches to resolve it. The title and discussion content initially only mentioned debounce, and didn't mention the noise issues and that the input was on the end of a long wire. Many people assume it's the same as a short wire, but it isn't. If it were a short wire, the problem would indeed be a solely debounce related one.

    The scenario is an input at the end of a long wire, in an environment that could be noisy.

    The situation could be better described as "remote switched input" or "remote line interfacing" perhaps; I don't know what the best technical term would be. In any case, you're interfacing _external_ hardware (a switch) to a computer's naked CMOS input (it has some protection built-in, but not a lot).

    Connecting things off-board is a more solution-level problem, whereas "debouncing" alone is local to the product.

    There are tons of solutions for remote connected devices to interface. A GPIO pin isn't (usually) a remote interface. Hardware is needed in-between. People often connect up I2C devices or long-wire outputs or switches off the end of meters of cable, directly to the GPIO, and 5 times out of 10 it might work for some of the time, and then even if it does work, then things might start misbehaving as the environment changes!

    The solution often involves some or all of these (this list is not exhaustive, it's all I could come up with for now):

    (1) implement debouncing (this is needed anyway even for a local switch on a board inside a product) either through software or hardware or a combination
    (2) noise reduction through (say) filtering; this too could partially be done in software, but clearly is feasible and often necessary with hardware too
    (3) increasing the noise immunity through greater hysteresis; this often involves using a schmitt trigger
    (4) increasing the noise immunity through greater voltage thresholds and lowering input impedance
    (5) preventing damage to the GPIO, through (say) ESD prevention parts, or electrical isolation

    People often want the cheap hardware option, which is to try to do it in software, but this is not always possible or desirable. If it's not possible then of course hardware is needed. But if it complicates the software to the point that it could introduce software errors, or severely restricts the way the code can be written to make it hard to maintain or extend, then this is an extremely compelling reason to add hardware.

    There are examples from the ham radio world.. this is the input for a Yaesu transceiver. You can see that they have tackled point (2) somewhat, and it will also help _slightly_ with point (1), which they are likely addressing with software debounce too.

    image

    Probably (I'm speculating) they are expecting higher-speed data on the input too. If they were not, then point (4) could be addressed a little bit by changing that 47k resistor to (say) 2.2k to greatly lower the impedance, and changing out that 1nF capacitor to at least 100nF (or even 1uF), if it's just a switch on the end for triggering a servo etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    It's not an entirely "debounce" problem. Debounce is just part of it. That's why you're seeing so many possible approaches to resolve it. The title and discussion content initially only mentioned debounce, and didn't mention the noise issues and that the input was on the end of a long wire. Many people assume it's the same as a short wire, but it isn't. If it were a short wire, the problem would indeed be a solely debounce related one.

    The scenario is an input at the end of a long wire, in an environment that could be noisy.

    The situation could be better described as "remote switched input" or "remote line interfacing" perhaps; I don't know what the best technical term would be. In any case, you're interfacing _external_ hardware (a switch) to a computer's naked CMOS input (it has some protection built-in, but not a lot).

    Connecting things off-board is a more solution-level problem, whereas "debouncing" alone is local to the product.

    There are tons of solutions for remote connected devices to interface. A GPIO pin isn't (usually) a remote interface. Hardware is needed in-between. People often connect up I2C devices or long-wire outputs or switches off the end of meters of cable, directly to the GPIO, and 5 times out of 10 it might work for some of the time, and then even if it does work, then things might start misbehaving as the environment changes!

    The solution often involves some or all of these (this list is not exhaustive, it's all I could come up with for now):

    (1) implement debouncing (this is needed anyway even for a local switch on a board inside a product) either through software or hardware or a combination
    (2) noise reduction through (say) filtering; this too could partially be done in software, but clearly is feasible and often necessary with hardware too
    (3) increasing the noise immunity through greater hysteresis; this often involves using a schmitt trigger
    (4) increasing the noise immunity through greater voltage thresholds and lowering input impedance
    (5) preventing damage to the GPIO, through (say) ESD prevention parts, or electrical isolation

    People often want the cheap hardware option, which is to try to do it in software, but this is not always possible or desirable. If it's not possible then of course hardware is needed. But if it complicates the software to the point that it could introduce software errors, or severely restricts the way the code can be written to make it hard to maintain or extend, then this is an extremely compelling reason to add hardware.

    There are examples from the ham radio world.. this is the input for a Yaesu transceiver. You can see that they have tackled point (2) somewhat, and it will also help _slightly_ with point (1), which they are likely addressing with software debounce too.

    image

    Probably (I'm speculating) they are expecting higher-speed data on the input too. If they were not, then point (4) could be addressed a little bit by changing that 47k resistor to (say) 2.2k to greatly lower the impedance, and changing out that 1nF capacitor to at least 100nF (or even 1uF), if it's just a switch on the end for triggering a servo etc.