Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum timer() question.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 412 subscribers
  • Views 1867 views
  • Users 0 members are here
  • flight simulator
  • nexgen
  • timer
  • arduino
Related

timer() question.

phoenixcomm
phoenixcomm over 3 years ago

Ok, that about says it all. what I need is a timer() which is set to 30,000 ms. (30 seconds). when I push a button to test the lights on the landing system, there are nine of them. I want to do the following:

for (int count = 0;  count < 9; count++ ){
digitalWrite( lamp[count], ON);}
timer = 300000 ms
return;

when timer = 0 set interrupt. 

for (int count = 0;  count < 9; count++ ){
digitalWrite( lamp[count], OFF);}
reset timer();
return;

That sound simple nope I don't want to stop what I am doing so a delay(30000) will not work.

  • Sign in to reply
  • Cancel

Top Replies

  • mayermakes
    mayermakes over 3 years ago +3
    the classic way is to use millis() to get the current time since boot and compare that to the last time you got millis()+target time if that has passed your timer has expired. so in the loop you first…
  • mayermakes
    mayermakes over 3 years ago +3
    the classic in short code: unsigned long startMillis; //some global variables available anywhere in the program unsigned long currentMillis; const unsigned long period = 1000; //the value is a number of…
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to mayermakes +3
    mayermakes Thanks Clem, I knew that somebody did this before I tried it. LOTS OF LOVE. Great programers don't write something new all the time... THEY JUST COPY IT!!!!
  • mayermakes
    mayermakes over 3 years ago

    the classic way is to use millis() to get the current time since boot and compare that to the last time you got millis()+target time if that has passed your timer has expired. so in the loop you first check on every loop and branch if the condition has been met.
    https://forum.arduino.cc/t/using-millis-for-timing-a-beginners-guide/483573
    but if you want to have arealyl simple solution here is library that does the same  in an easier way: github.com/.../neotimer

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 3 years ago

    the classic in short code:

    unsigned long startMillis;  //some global variables available anywhere in the program
    unsigned long currentMillis;
    const unsigned long period = 1000;  //the value is a number of milliseconds
    const byte ledPin = 13;    //using the built in LED
    
    void setup()
    {
      Serial.begin(115200);  //start Serial in case we need to print debugging info
      pinMode(ledPin, OUTPUT);
      startMillis = millis();  //initial start time
    }
    
    void loop()
    {
      currentMillis = millis();  //get the current "time" (actually the number of milliseconds since the program started)
      if (currentMillis - startMillis >= period)  //test whether the period has elapsed
      {
        digitalWrite(ledPin, !digitalRead(ledPin));  //if so, change the state of the LED.  Uses a neat trick to change the state
        startMillis = currentMillis;  //IMPORTANT to save the start time of the current LED state.
      }
    }

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to mayermakes

     mayermakes  Thanks Clem, I knew that somebody did this before I tried it.  LOTS OF LOVE. Great programers don't write something new all the time... THEY JUST COPY IT!!!! 

    • Cancel
    • Vote Up +3 Vote Down