Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Output Multiplier
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 413 subscribers
  • Views 191 views
  • Users 0 members are here
Related

Arduino Output Multiplier

tabarus12
tabarus12 over 13 years ago

Hey guys, I have this cool output miltiplier that can hold memory and be expanded to any size tha uses shift registers and D type flip flops but I am having trouble finding something to use it for.

Any body got any idea on what to apply it?.

Im thinking robotics but Im not shure, I attache a video sample of the multiplier and the schematic in case anyone wants to build it and send feedback.

 

Here is a test code for the miltiplier, common pin is the arduino negative.

 

#include<Streaming.h>

 

int data = 3; //Declare data pin//

int clk = 4; //Declare clock pin//

int buf = 5; //Declare buffer enable pin//

 

int c = 1; //Declare counter variable//

int i = 1; //Declare intial position variable//

int s = 24; //Declare stop position variable//

int d = 1; //Declare data variable//

int t = 20 ; //Declare time variable//

 

void setup() {

  pinMode(data, OUTPUT); //Set data pin to output//

  pinMode(clk, OUTPUT); //Set clock pin to output//

  pinMode(buf, OUTPUT); //Set buffer enable pin to output//

 

  Serial.begin(9600); //Start serial port transmition//

}

 

void loop() {

  for(d=i; d<=s; d++) { //Increase data variable//

    Input(); //Call for sequence run//

    Serial << "Data Place is: " << d << endl; //Print data to serial port//

    digitalWrite(buf, HIGH); //Set buffer enable to 1//

    digitalWrite(buf, LOW); //Set buffer enable to 0//

  }

 

  for(d=s; d>=i; d--) { //Decrease data variable//

    Input(); //Call for sequence run//

    Serial << "Data Place is: " << d << endl; //Print data to serial port//

    digitalWrite(buf, HIGH); //Set buffer enable to 1//

    digitalWrite(buf, LOW); //Set buffer enable to 0//

  }

}

 

void Data() { //Data print routine//

    if(c==d) { //When counter equals data position//

      digitalWrite(data, HIGH); //set data pin to 1//

    }

    else { //On data and conter not match//

      digitalWrite(data, LOW); //Set data pin to 0//

    }

}

 

void Input() { //Buffer run routine//

  for( c=1; c<=s; c++) { //Increase counter to last position//

    Data(); //Call for data print routine//

    digitalWrite(clk, HIGH); //Set clock pin to 1//

    delay(t); //Delay betwen steps//

    digitalWrite(clk, LOW); //Set clock pin to 0//

  }

  c=1; //Return counter to 1//

}

Attachments:
image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • tabarus12
    tabarus12 over 13 years ago

    Ok, since there was no food for thought I decided to go for robotics and autmation, Ive just finished building a power driver for an EDGE toy robot arm Ill upload video of it working once Ive tested and perfected the sketch for it, it so cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tabarus12
    tabarus12 over 13 years ago

    Ok, since there was no food for thought I decided to go for robotics and autmation, Ive just finished building a power driver for an EDGE toy robot arm Ill upload video of it working once Ive tested and perfected the sketch for it, it so cool.