Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Custom i2c with Arduino UNO.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 410 subscribers
  • Views 2037 views
  • Users 0 members are here
  • ports
  • i2c
  • programming
  • uno
  • pinout
  • arduino
Related

Custom i2c with Arduino UNO.

A_N_T_O_N
A_N_T_O_N over 3 years ago

For educational purposes, I would like to write my own i2c protocol. Is it possible to write a custom i2c library to communicate using regular ports, or should I use the SCL and SDA ports? Do the SCL/SDA ports have special hardware implementations, or can you configure any port for i2c?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +1
    SCL/SDA are open drain outputs. (SDA can also be an input) If a digital pin can be configured as an open drain output, possibly with an internal pull-up resistor, it can be used for a custom I2C implementation…
  • beacon_dave
    beacon_dave over 3 years ago +1
    A_N_T_O_N said: Do the SCL/SDA ports have special hardware implementations The microcontroller datasheet is useful for that sort of information.
  • dougw
    dougw over 3 years ago +1
    You could use any digital output as an open drain output if you add a FET to the output, but it is tricky to use the same pin for input.
Parents
  • dougw
    dougw over 3 years ago

    SCL/SDA are open drain outputs. (SDA can also be an input) If a digital pin can be configured as an open drain output, possibly with an internal pull-up resistor, it can be used for a custom I2C implementation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    SCL/SDA are open drain outputs. (SDA can also be an input) If a digital pin can be configured as an open drain output, possibly with an internal pull-up resistor, it can be used for a custom I2C implementation.