Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Seting up motor on limit switches
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 410 subscribers
  • Views 1805 views
  • Users 0 members are here
Related

Seting up motor on limit switches

Vallka
Vallka over 2 years ago

Hello, I am new to all this but am learning and really enjoying it.

I have been working on a project to turn a machine with a motor for a time period then stop and wait for a tiime period then repeat.

This is not working out so I want to change the plan and make it work on a button/motion sensor and limit switches.

This is the code I have and I had alot of help from others on this.

Ideally you would push a button, the motor would run for a time period or hit limit swich then reverse for a time period and stop until button pushed again.

This is the code I have.

// run forwards for 10sec
// stop for 2sec
// reverse for 10sec,
// stop for 3min
// repeat the loop endlessly.

int r_en = 2;
int l_en = 3;
int r_pwm = 5;
int l_pwm = 6;



void setup() {
pinMode(r_en, OUTPUT);
pinMode(l_en, OUTPUT);
pinMode(r_pwm, OUTPUT);
pinMode(l_pwm, OUTPUT);
}
void loop() {
forward();
delay(10000);
stop();
delay(2000); 
reverse();
delay (10000);
stop();
delay (3 * 60 * 1000); 
}

void stop() {
analogWrite(r_pwm, 0);
analogWrite(l_pwm, 0);
digitalWrite(r_en, LOW); // disable r motor
digitalWrite(l_en, LOW); // disable l motor
}

void forward() {
analogWrite(r_pwm, 150);
analogWrite(l_pwm, 0);
digitalWrite(r_en, HIGH); // enable motor r
digitalWrite(l_en, HIGH); // enable motor l
}

void reverse() {
analogWrite(r_pwm, 0);
analogWrite(l_pwm, 150);
digitalWrite(r_en, HIGH); // enable motor r
digitalWrite(l_en, HIGH); // enable motor l
}

  • Sign in to reply
  • Cancel

Top Replies

  • aspork42
    aspork42 over 2 years ago +1
    Hello, In your subroutines like forward() , the code just runs through the four lines one time, then returns to the main loop. I’m not in front of an arduino to check, but I think that they delay() function…
  • balajivan1995
    balajivan1995 over 2 years ago +1
    I'm assuming you want to add two more input to control the flow of motor instead of coding the sequence to run one event after another. Below is the rough idea of how to implement it. void process_motor…
Parents
  • aspork42
    aspork42 over 2 years ago

    Hello,

    In your subroutines like forward() , the code just runs through the four lines one time, then returns to the main loop. I’m not in front of an arduino to check, but I think that they delay() function will pause the PWM output. So you may need to wrap your subroutine with a while() loop and count the time.

    Another think I do when I encounter things like this is just start a blank sketch and include /only/ the code required for one basic step of my program. Then you can check manually if you can even run the motor without any fancy logic at all - just PWM and the enable signals. Then add in complexity like the delay, and then the other motor moves.

    *Edit - documentation indicates that PWM should be maintained during delay; but it still isn’t best practice to use delay function for more than 10’s of ms.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • aspork42
    aspork42 over 2 years ago

    Hello,

    In your subroutines like forward() , the code just runs through the four lines one time, then returns to the main loop. I’m not in front of an arduino to check, but I think that they delay() function will pause the PWM output. So you may need to wrap your subroutine with a while() loop and count the time.

    Another think I do when I encounter things like this is just start a blank sketch and include /only/ the code required for one basic step of my program. Then you can check manually if you can even run the motor without any fancy logic at all - just PWM and the enable signals. Then add in complexity like the delay, and then the other motor moves.

    *Edit - documentation indicates that PWM should be maintained during delay; but it still isn’t best practice to use delay function for more than 10’s of ms.