Arduino
  • Products
  • More
Arduino
Arduino Forum Getting 4.2V from Arduino UNO using voltage divder resistor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 412 subscribers
  • Views 3396 views
  • Users 0 members are here
  • voltage divider
  • arduino
Related

Getting 4.2V from Arduino UNO using voltage divder resistor

aswinth
aswinth over 1 year ago

Hi i am a completely new to electronics so please be gentle. 

I just got an arduino uno board and a GSM module called sim800A. I came to know that I should power the GSM module with 4.2V, but Arduino only provides 3.3V and 5V as power output. After looking into ways to convert 5V to 4.2V I came to know that i can use a voltage divider circuit.

Now I understand how a voltage divider circuit works. So i need to connect two resistors to 5V of Arduino to get 4.2V. I am using this below voltage divider calculator to calculate the values of my resistor.

circuitdigest.com/.../voltage-divider-calculator

I have kept the Vin voltage as 5V that i will get from Arduino and output voltage as 4.2V. I already have 1000 ohms (1k ohms) so i am using that for R1 now the result is like this 

image

It is telling me to use 1941 ohms for R2, but there is no resistor with that value. I tired changing the value of R1 and calculate again. But still i am not getting whole numbers value for R2. Can some one help me what i should do here. I am very far from local electronic market so don't have much resistor values with me. 

  • Sign in to reply
  • Cancel

Top Replies

  • aswinvenu
    aswinvenu over 1 year ago +2 verified
    Hi Aswinth, Voltage dividers are not really useful if you want to deliver power to a circuit ( You can compute current by V/(R1+R2)). You can use LDOs or DCDC power supply. https://simcom.ee/documents…
  • robogary
    robogary over 1 year ago +2
    ROFL - I will be gentle I use a ton of these adjustable LM2596 buck power supplies, link provided as an example. I usually use them on projects with a battery, 12V or 7V , to provide a regulated…
  • aswinth
    aswinth over 1 year ago in reply to aswinvenu +2
    Thank you, this is exactly what I needed. I used a 12V 2A adapter and built a regulator. i dint use MIC29302 but LM317 instead Thanks
Parents
  • aswinvenu
    +1 aswinvenu over 1 year ago

    Hi Aswinth,

    Voltage dividers are not really useful if you want to deliver power to a circuit ( You can compute current by V/(R1+R2)). You can use LDOs or DCDC power supply.
    https://simcom.ee/documents/SIM800A/SIM800A_Hardware%20Design_V1.02.pdf page number 19. You need a good 2A current source for powering the module.

    image

    You can use LM317 as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • aswinvenu
    +1 aswinvenu over 1 year ago

    Hi Aswinth,

    Voltage dividers are not really useful if you want to deliver power to a circuit ( You can compute current by V/(R1+R2)). You can use LDOs or DCDC power supply.
    https://simcom.ee/documents/SIM800A/SIM800A_Hardware%20Design_V1.02.pdf page number 19. You need a good 2A current source for powering the module.

    image

    You can use LM317 as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • aswinth
    0 aswinth over 1 year ago in reply to aswinvenu

    Thank you, this is exactly what I needed. I used a 12V 2A adapter and built a regulator. i dint use MIC29302 but LM317 instead

    Thanks

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 1 year ago in reply to aswinth

    Another satisfied customer who shopped the E14 Community.