Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Multi Toggle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 412 subscribers
  • Views 1490 views
  • Users 0 members are here
Related

Multi Toggle

Gary.Baker
Gary.Baker over 1 year ago
CAN SOMEONE WITH MORE EXPERIENCE THAN ME HELP WITH THE MISTAKE WITH THIS CODE.
THE PROBLEM IS THAT EITHER PINS 2 OR 3 WILL TOGGLE PINS 12 OR 13.
WHAT I WANT IS PNE 2 TOGGLE PIN 12 AND PIN 3 TOGGLE PIN 13
THANKS. GARY
/*
Button

The circuit:
- LED attached from pin 13 to ground through 220 ohm resistor
- pushbutton attached to pin 2 from +5V
- 10K resistor attached to pin 2 from ground

- Note: on most Arduinos there is already an LED on the board
attached to pin 13.

*/

// constants won't change. They're used here to set pin numbers:
const int buttonPin2 = 2; // the number of the pushbutton pin
const int ledPin13 = 13; // the number of the LED pin
const int buttonPin3 = 3; // the number of the pushbutton pin
const int ledPin12 = 12; // the number of the LED pin

// variables will change:
int buttonState2 = 0; // variable for reading the pushbutton status
int buttonState3 = 0; // variable for reading the pushbutton status
void setup() {
// initialize the LED pin as an output:
pinMode(ledPin13, OUTPUT);
// initialize the pushbutton pin as an input:
pinMode(buttonPin2, INPUT);
// initialize the LED pin as an output:
pinMode(ledPin12, OUTPUT);
// initialize the pushbutton pin as an input:
pinMode(buttonPin3, INPUT);
}

void loop() {
// read the state of the pushbutton value:
buttonState2 = digitalRead(buttonPin2);

// check if the pushbutton is pressed. If it is, the buttonState is HIGH:
if (buttonState2 == HIGH) {
digitalWrite(13, !digitalRead(13)); // toggle state
delay(500); // wait around for 1 sec (1000 ms)
}



// read the state of the pushbutton value:
buttonState3 = digitalRead(buttonPin3);

// check if the pushbutton is pressed. If it is, the buttonState is HIGH:
if (buttonState3 == HIGH) {
digitalWrite(12, !digitalRead(12)); // toggle state
delay(500); // wait around for 1 sec (1000 ms)

}else {
}
}
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago +3
    A few points: (1) When entering code, please use the insert code menu item, so that it's properly formatted. You'll get less people helping if you make it hard for them to see your code properly. …
  • shabaz
    shabaz over 1 year ago +2
    How AI would do it, with some prodding: // toggle.ino // rev 0.1 // buttons with pull-downs on pins 2 and 3 are to toggle outputs on pins 12 and 13 respectively // buttons are connected to the microcontroller…
  • robogary
    robogary over 1 year ago +2
    I myself being a self admitted coding dunderhead, avoid the use of inversion in this case because its easy to overlook. I'd use direct commands if buttonState3 == HIGH then {digitalWrite (12, LOW) ;…
Parents
  • hardip
    hardip over 1 year ago

    const int buttonPin2 = 2; // the number of the pushbutton pin
    const int ledPin13 = 13; // the number of the LED pin
    const int buttonPin3 = 3; // the number of the pushbutton pin
    const int ledPin12 = 12; // the number of the LED pin
    
    volatile byte state12 = LOW;  // variable that will be updated in the ISR
    volatile byte state13 = LOW;  // variable that will be updated in the ISR
    
    int prev_12=0;
    int prev_13=0;
    
    void pin12(){state12 = !state12;}
    void pin13(){state13 = !state13;}
    
    void setup() {
      pinMode(buttonPin2, INPUT_PULLUP);
      pinMode(ledPin13, OUTPUT);
      pinMode(buttonPin3, INPUT_PULLUP);
      pinMode(ledPin12, OUTPUT);
    
      attachInterrupt(digitalPinToInterrupt(buttonPin2), pin12, RISING);
      attachInterrupt(digitalPinToInterrupt(buttonPin3), pin13, RISING);
    }
    
    void loop() {
      if(prev_12 != state12 || prev_13 != state13){
        prev_12 = state12;
        prev_13 = state13;
        digitalWrite(ledPin12,state12);
        digitalWrite(ledPin13,state13);}
        delay(100);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hardip
    hardip over 1 year ago

    const int buttonPin2 = 2; // the number of the pushbutton pin
    const int ledPin13 = 13; // the number of the LED pin
    const int buttonPin3 = 3; // the number of the pushbutton pin
    const int ledPin12 = 12; // the number of the LED pin
    
    volatile byte state12 = LOW;  // variable that will be updated in the ISR
    volatile byte state13 = LOW;  // variable that will be updated in the ISR
    
    int prev_12=0;
    int prev_13=0;
    
    void pin12(){state12 = !state12;}
    void pin13(){state13 = !state13;}
    
    void setup() {
      pinMode(buttonPin2, INPUT_PULLUP);
      pinMode(ledPin13, OUTPUT);
      pinMode(buttonPin3, INPUT_PULLUP);
      pinMode(ledPin12, OUTPUT);
    
      attachInterrupt(digitalPinToInterrupt(buttonPin2), pin12, RISING);
      attachInterrupt(digitalPinToInterrupt(buttonPin3), pin13, RISING);
    }
    
    void loop() {
      if(prev_12 != state12 || prev_13 != state13){
        prev_12 = state12;
        prev_13 = state13;
        digitalWrite(ledPin12,state12);
        digitalWrite(ledPin13,state13);}
        delay(100);
    }