Arduino Forum wireless video feed Arduino
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
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 460 views
  • Users 0 members are here
  • arduino uno
  • x bee
  • wireless;
  • arduino
  • arduino-shield
Related

wireless video feed Arduino

Former Member
Former Member over 9 years ago

Hello,

 

I was wondering if it was possible to use arduino camera module to send live video feed.

Can i use X bee modules to do so? I want the video input from one arduino, send it to the other arduino and display it on a screen.

 

can i display this feed on an lcd screen module??

 

please suggest a method by which i can achieve this.

reply would be greatly appreciated.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • Problemchild
    Problemchild over 9 years ago in reply to shabaz +3
    If you ask enough times you'll get the answer apparently What's this obsession with the Arduino anyway? use something a bit bigger! it's like those stories of 27 people on a scooter..yes you can do it…
  • COMPACT
    COMPACT over 9 years ago +1
    Of course you can but you'll have to be the one to work it out! I was told I couldn't drive 3,072 colour LEDs and display full 24fps video from a single microcontroller but demonstrated that it could.
  • clem57
    clem57 over 9 years ago in reply to COMPACT +1
    COMPACT The engine that could! Clem
  • shabaz
    shabaz over 9 years ago

    Repeat of a question you asked a week ago..

    With some clever engineering, external buffers, slow frame rate, it might be possible but generally the answer is no.

    More info in the other post where you asked this question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago

    Of course you can but you'll have to be the one to work it out!

     

    I was told I couldn't drive 3,072 colour LEDs and display full 24fps video from a single microcontroller but demonstrated that it could.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to COMPACT

    COMPACT

         The engine that could!

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 9 years ago in reply to COMPACT

    Surely you are clocking 3072Leds  x 8 bitsx3(RGB) x24fps or 1.769 Mbits per second . Most chains seem to support of the order of 2MBits so you could even do it in a single chain if you were lucky or better still several chains to reduce the clk rate required.  it all depends on what you were doing and what the micro controller was

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 9 years ago in reply to shabaz

    If you ask enough times you'll get the answer apparently image

    What's this obsession with the Arduino anyway? use something a bit bigger! it's like those stories of 27 people on a scooter..yes you can do it but it aint clever and it still isnt a bus!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to Problemchild

    Nope! The LEDS have a set protocol that operate at a maximum of 800kHz.