Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino device unused I/O's...... what to do with them?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 413 subscribers
  • Views 509 views
  • Users 0 members are here
  • Design
  • arduino
Related

Arduino device unused I/O's...... what to do with them?

colporteur
colporteur 6 months ago

What is the best practice for unused Arduino device I/O pins, connect them to ground or Vcc? If not connected on the PCB what if anything do you do with them in code?

My go to bathroom reading material is The Art of Electronics Paul Horowitz & Winfield Hill. I just read a section on routine design considerations. "No open inputs" is the suggestion. It was a discussion on CMOS design but the commentary got me to thinking about Arduino's. 

I've never done anything with them. I assumed they were conditioned in the device.

For No Open Inputs planning, I wonder how the pro's in E14 handle it.

  • Sign in to reply
  • Cancel

Top Replies

  • vmate
    vmate 6 months ago +2
    You shouldn't need to do anything with it. They would default to the high-impedance INPUT state, but it shouldn't be an issue at all, since you're not actually reading them. If you're paranoid, set all…
Parents
  • vmate
    vmate 6 months ago

    You shouldn't need to do anything with it. They would default to the high-impedance INPUT state, but it shouldn't be an issue at all, since you're not actually reading them. If you're paranoid, set all of them to INPUT_PULLUP, which will activate an internal pullup resistor in the MCU to make sure they are always HIGH.

    The 'no floating inputs' guideline is a good one to keep in mind, but it's mostly related to analog ICs and circuits. Microcontrollers will essentially shut down all the logic 'behind' an unused input pin, so they won't really affect anything at all.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vmate
    vmate 6 months ago

    You shouldn't need to do anything with it. They would default to the high-impedance INPUT state, but it shouldn't be an issue at all, since you're not actually reading them. If you're paranoid, set all of them to INPUT_PULLUP, which will activate an internal pullup resistor in the MCU to make sure they are always HIGH.

    The 'no floating inputs' guideline is a good one to keep in mind, but it's mostly related to analog ICs and circuits. Microcontrollers will essentially shut down all the logic 'behind' an unused input pin, so they won't really affect anything at all.