Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Anyone Have stability issues with Arduino Uno Q?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 411 subscribers
  • Views 1570 views
  • Users 0 members are here
  • On the line design challenge
  • arduino uno q
  • arduino
Related

Anyone Have stability issues with Arduino Uno Q?

SensoredHacker0
SensoredHacker0 6 months ago

So im at my PC typing away. The Uno Q ran my code on the first try on the first day i got it, a couple days ago.
made some more tests, for 2 days everything was working great. Then, without warning, did not move it, or touch it, it stopped.
ok fine I guess. Then I tried to upload new test code. it compiles, and claims to have been uploaded. but the code doesnt work. 


The hardware which was attached, when it failed:
a Max33041E shield, and the Ethernet R3 shield. these had been working for a couple days straight. 

Not like the code is buggy, but like it doesn't even init the serial print lines. 
bash my head on the wall for a while. 
Press Reset. nothing. Un plug it, wait, re insert usb power.
$dmesg shows it, loading without issue.  

Pull the shields off, load blink. same thing, it compiles, and claims to upload, but the code never runs. 

I haven't reinstalled the boot-loader, by the time I thought to try that, I'd already gone to bed. 
But I've never had such random problems before. Ive got arduino running in projects that have run for 6 years straight not problem.

besides reloading the bootloader and one have some ideas?


Are there stability issues with the Arduino Uno Q I should know about?

Perhaps the most frustrating thing was that the LED matrix was making little hearts and arduino logos the whole time. 
meanwhile blink wont run. 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz 6 months ago in reply to ralphjy +4
    I'm glad you guys are investigating the Q and working through the issues. It will help everyone. However, got to strongly disagree with this: The Q can't really be expected to be compared reliability…
  • ralphjy
    ralphjy 6 months ago +3
    The Q can't really be expected to be compared reliability/stability wise with previous Arduinos. With the new hybird MPU/MCU structure it is going to have a lot more issues than the MCU only boards. I…
  • ralphjy
    ralphjy 6 months ago in reply to shabaz +2
    I agree with your comments, but just to clarify what I meant - the Q has much more complexity and many more points of failure, both in hardware and software. I do think the current implementation is faulty…
Parents
  • ralphjy
    ralphjy 6 months ago

    The Q can't really be expected to be compared reliability/stability wise with previous Arduinos.  With the new hybird MPU/MCU structure it is going to have a lot more issues than the MCU only boards.  I have found that I encountered different sets of issues depending on the hardware and software configuration and development environment.  You really haven't indicated how you are set up (PC USB host, headless, standalone), how you are powered, and what your development setup is. 

    Based on your description, I assume that you are using AppLab running on a USB host.  How are you determining that it doesn't reach the serial print lines (that would be Monitor rather than Serial in AppLab)?  Your Linux side appears to be running (assume you checked dmesg via ssh).  If you are in AppLab I would guess that the RouterBridge is failing and may be hanging the MCU.  The AppLab Blink example no longer runs only on the MCU.

    I would recommend that you connect a USB to UART adapter (3.3V) between your PC and the MCU.  You could also try one (1.8V) between the PC and the MPU.  That would help with debug.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy 6 months ago

    The Q can't really be expected to be compared reliability/stability wise with previous Arduinos.  With the new hybird MPU/MCU structure it is going to have a lot more issues than the MCU only boards.  I have found that I encountered different sets of issues depending on the hardware and software configuration and development environment.  You really haven't indicated how you are set up (PC USB host, headless, standalone), how you are powered, and what your development setup is. 

    Based on your description, I assume that you are using AppLab running on a USB host.  How are you determining that it doesn't reach the serial print lines (that would be Monitor rather than Serial in AppLab)?  Your Linux side appears to be running (assume you checked dmesg via ssh).  If you are in AppLab I would guess that the RouterBridge is failing and may be hanging the MCU.  The AppLab Blink example no longer runs only on the MCU.

    I would recommend that you connect a USB to UART adapter (3.3V) between your PC and the MCU.  You could also try one (1.8V) between the PC and the MPU.  That would help with debug.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz 6 months ago in reply to ralphjy

    I'm glad you guys are investigating the Q and working through the issues. It will help everyone.

    However, got to strongly disagree with this:

    The Q can't really be expected to be compared reliability/stability wise with previous Arduinos.  With the new hybird MPU/MCU structure it is going to have a lot more issues than the MCU only boards.

    That may be the current reality with Q, but is in no way normal. I believe it means that the Arduino people have either (a) treated their creation like a Linux server or desktop PC device, or (b) is simply buggy in their implementation. Either way it's a showstopper as far as I can see.  It's frustrating, I would love to use the Q but not if it cannot be power-cycled with confidence.

    This is not the first device containing a microprocessor and microcontroller, and it needs to start up consistently every single time. I'd be especially concerned if the cause is (a) because then that means there's a complete misunderstanding by them about how people use any typical SBC or any Arduino board for that matter.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 6 months ago in reply to shabaz

    I agree with your comments, but just to clarify what I meant - the Q has much more complexity and many more points of failure, both in hardware and software.  I do think the current implementation is faulty and hopefully that will be fixed in time.   

    You're smart to wait for things to settle down, I expect many of the issues to be resolved in the next couple of quarters.  And the media interface should be available soon.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo 6 months ago in reply to shabaz

    A bit aside, but I see the Opta in the same category of "not ready for prime time".  I have one.  It's too quirky.  It's not what I consider "Arduino" - which, to me, infers stable and well supported (both by the company and the community).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • SensoredHacker0
    SensoredHacker0 6 months ago in reply to kmikemoo

    When ever Opta first came out, my employer wanted desperately to switch. but all the devices you might want to interface with were locked out. I wrote to Arduino and they said they were concerned about licensing, which amounted to a locked down open platform. as I understand it, that has improved over time, but still, we couldn't adopt it. if anyone is going to transition, to some other system, that system either needs support for other devices, or needs to have devices that offer the missing functionality.  Arduino Opta had neither.