Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Are you looking out for the Arduino Ventuno Q?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 413 subscribers
  • Views 3385 views
  • Users 0 members are here
  • npu
  • ai model
  • qualcomm
  • VENTUNO Q
  • arduino
Related

Are you looking out for the Arduino Ventuno Q?

cstanton
cstanton 5 months ago

How on the heels of the Arduino Uno Q, the new offering in conjunction with Qualcomm is the Arduino Ventuno Q:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here's a run down of the specifications:

  • Main Processor (MPU): Qualcomm Dragonwing IQ‑8275 (octa‑core Arm CPU with Adreno 623 GPU and AI accelerator up to ~40 TOPS)
  • Microcontroller (MCU): STM32H5F5 (Arm Cortex‑M33 running at ~250 MHz)
  • MCU Memory: 4 MB Flash, 1.5 MB RAM
  • System Memory: 16 GB LPDDR5 RAM
  • Onboard Storage: 64 GB eMMC
  • Storage Expansion: M.2 slot (NVMe SSD support, PCIe Gen 4)
  • Wireless Connectivity: Wi‑Fi 6 (2.4 / 5 / 6 GHz), Bluetooth 5.3
  • Wired Networking: 2.5 Gigabit Ethernet (RJ45)
  • USB Ports:
    • 1 × USB‑C (power, data, DisplayPort Alt Mode)
    • 2 × USB 3.0 Type‑A
  • GPIO & Expansion:
    • 40‑pin GPIO header (Raspberry Pi compatible)
    • Arduino UNO‑style shield compatibility
    • Qwiic / I²C connectors
  • Camera Support: Up to 3 × MIPI‑CSI camera interfaces
  • Display Outputs:
    • HDMI
    • MIPI‑DSI
    • USB‑C DisplayPort Alt Mode
  • Audio: Microphone input and audio output via onboard headers
  • Industrial Interfaces: Multiple CAN‑FD interfaces (with and without PHY)
  • Power Input:
    • USB‑C: 5V up to 3A
    • Barrel jack: 12–24V DC
    • Screw terminal: 7–24V DC
  • Dimensions: Approximately 160 × 100 × 25.8 mm
  • Software Support: Linux (Ubuntu / Debian) on MPU and Arduino-compatible environment (Zephyr-based) on MCU

I've forwarded a few of my own questions to Arduino that I'll post to the element14 Community, mainly revolving around what's supported over the HDMI and DisplayPort, along with a 'high speed connector' it has available (and how that's used), but what we'd really like is to get some of these into your hands - maybe as a RoadTest or some kind of experimenting with competition.

I'm seeing a lot of microcontroller boards that straddle microcontroller hardware now, especially that they run 'ai models', but I'm not sure that people have gotten to grips with this yet, what's your level of working with them?

The answers from this will help us to tailor content from Arduino for the Community.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw 5 months ago +2
    Probably not what it is aimed at but what I might try to use it for is capturing picture-in-picture video blogs.
  • michaelkellett
    michaelkellett 5 months ago +2
    It's very hard to see where Qualcomm are going with Arduino. It's moved a very long way from the Arduino origins. The Ventuno doesn't seem to be aimed at industrial or commercial projects (stuck with…
  • kk99
    kk99 5 months ago +2
    I have registered for notification when it will be available. I am looking for a board that has support for NVMe and USB-C Display Mode. It may be good to try something different than Raspberry with hardware…
Parents
  • robogary
    robogary 5 months ago

    After reading some replies, I' m a bit perplexed too, at the commercial strategy, and at the same time I'm overwhelmed with possibilities. 

    Is Ventuno launch meant as an open source product to help enlighten the world, or an eval platform to use Qualcomm ICs or a mass produced product to embed in embedded solutions ? 

    3 camera inputs using YOLO-X would be an incredible show and tell demonstration for inspiring young creative minds. I'd like to start implementing now, :-) except Im on the slow boat just to use one camera. The tool better help me with examples like the Arduino tool does for driving servos and ping modules.

    Id love to put object detection on my hobby projects. My Spring Clean Garden Guardian project would be so much better with a visual deer recognition on it. I imagine showing kids a "sibling detector" alarm they can build with a Webcam and importing a few pics of their sibling. My bucket list project is to use object detection for vehicle steering. Does Ventuno help me provide basic solutions fairly quickly ? 

    I for sure would like to give it a spin. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary 5 months ago

    After reading some replies, I' m a bit perplexed too, at the commercial strategy, and at the same time I'm overwhelmed with possibilities. 

    Is Ventuno launch meant as an open source product to help enlighten the world, or an eval platform to use Qualcomm ICs or a mass produced product to embed in embedded solutions ? 

    3 camera inputs using YOLO-X would be an incredible show and tell demonstration for inspiring young creative minds. I'd like to start implementing now, :-) except Im on the slow boat just to use one camera. The tool better help me with examples like the Arduino tool does for driving servos and ping modules.

    Id love to put object detection on my hobby projects. My Spring Clean Garden Guardian project would be so much better with a visual deer recognition on it. I imagine showing kids a "sibling detector" alarm they can build with a Webcam and importing a few pics of their sibling. My bucket list project is to use object detection for vehicle steering. Does Ventuno help me provide basic solutions fairly quickly ? 

    I for sure would like to give it a spin.