Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Are you looking out for the Arduino Ventuno Q?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 413 subscribers
  • Views 3352 views
  • Users 0 members are here
  • npu
  • ai model
  • qualcomm
  • VENTUNO Q
  • arduino
Related

Are you looking out for the Arduino Ventuno Q?

cstanton
cstanton 5 months ago

How on the heels of the Arduino Uno Q, the new offering in conjunction with Qualcomm is the Arduino Ventuno Q:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here's a run down of the specifications:

  • Main Processor (MPU): Qualcomm Dragonwing IQ‑8275 (octa‑core Arm CPU with Adreno 623 GPU and AI accelerator up to ~40 TOPS)
  • Microcontroller (MCU): STM32H5F5 (Arm Cortex‑M33 running at ~250 MHz)
  • MCU Memory: 4 MB Flash, 1.5 MB RAM
  • System Memory: 16 GB LPDDR5 RAM
  • Onboard Storage: 64 GB eMMC
  • Storage Expansion: M.2 slot (NVMe SSD support, PCIe Gen 4)
  • Wireless Connectivity: Wi‑Fi 6 (2.4 / 5 / 6 GHz), Bluetooth 5.3
  • Wired Networking: 2.5 Gigabit Ethernet (RJ45)
  • USB Ports:
    • 1 × USB‑C (power, data, DisplayPort Alt Mode)
    • 2 × USB 3.0 Type‑A
  • GPIO & Expansion:
    • 40‑pin GPIO header (Raspberry Pi compatible)
    • Arduino UNO‑style shield compatibility
    • Qwiic / I²C connectors
  • Camera Support: Up to 3 × MIPI‑CSI camera interfaces
  • Display Outputs:
    • HDMI
    • MIPI‑DSI
    • USB‑C DisplayPort Alt Mode
  • Audio: Microphone input and audio output via onboard headers
  • Industrial Interfaces: Multiple CAN‑FD interfaces (with and without PHY)
  • Power Input:
    • USB‑C: 5V up to 3A
    • Barrel jack: 12–24V DC
    • Screw terminal: 7–24V DC
  • Dimensions: Approximately 160 × 100 × 25.8 mm
  • Software Support: Linux (Ubuntu / Debian) on MPU and Arduino-compatible environment (Zephyr-based) on MCU

I've forwarded a few of my own questions to Arduino that I'll post to the element14 Community, mainly revolving around what's supported over the HDMI and DisplayPort, along with a 'high speed connector' it has available (and how that's used), but what we'd really like is to get some of these into your hands - maybe as a RoadTest or some kind of experimenting with competition.

I'm seeing a lot of microcontroller boards that straddle microcontroller hardware now, especially that they run 'ai models', but I'm not sure that people have gotten to grips with this yet, what's your level of working with them?

The answers from this will help us to tailor content from Arduino for the Community.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw 5 months ago +2
    Probably not what it is aimed at but what I might try to use it for is capturing picture-in-picture video blogs.
  • michaelkellett
    michaelkellett 5 months ago +2
    It's very hard to see where Qualcomm are going with Arduino. It's moved a very long way from the Arduino origins. The Ventuno doesn't seem to be aimed at industrial or commercial projects (stuck with…
  • kk99
    kk99 5 months ago +2
    I have registered for notification when it will be available. I am looking for a board that has support for NVMe and USB-C Display Mode. It may be good to try something different than Raspberry with hardware…
Parents
  • veluv01
    veluv01 4 months ago

    A Webinar(adding along with a AMA session, since it's a new hardware) followed by a RoadTest seems like a interesting option.Sweat smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • veluv01
    veluv01 4 months ago

    A Webinar(adding along with a AMA session, since it's a new hardware) followed by a RoadTest seems like a interesting option.Sweat smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • veluv01
    veluv01 4 months ago in reply to veluv01

    I'm more inclined towards using it for running Local LLM Agents, since it got decent amount of RAM(16 GB); it can run upto 14b parameter models and power consumption is within 15W.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton 4 months ago in reply to veluv01

    Do you have experience with running local llm agents?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate 4 months ago in reply to veluv01

    RAM bandwidth is not looking that great for LLMs (about 50 GB/s if my math is right), I guess some 2B active MoE would be fine even on slow RAM, but probably not a pleasant experience. 

    Also, I can't see any detailed specs on the CPU cores or NPU either, so hard to tell how fast prefill/prompt processing would go.

    I don't know of any recent MoE models that would be a good fit off the top of my head, Qwen1.5-MoE-A2.7B looks like a good option but it's old, or Gemma 4 12B is newer but dense. It would be fun to experiment with these in a RoadTest though.

    The real killer would be Qwen3.6-35B-A3B on a 32GB variant.