Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum What is your take on Qualcomm Arduino becoming Persona Non Grata
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 413 subscribers
  • Views 629 views
  • Users 0 members are here
  • qualcomm
  • arduino_projects
  • arduino
Related

What is your take on Qualcomm Arduino becoming Persona Non Grata

colporteur
colporteur 28 days ago

I'm a big Arduino fan. I recall the purchase announcement.

I chimed in at the time but I've been sidelined for the last year on microcontroller project so I have to experience to speak of.

https://toolguyd.com/qualcomm-arduino-has-become-persona-non-grata/

I read this article and thought E14 peoples could share their insight.

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy 27 days ago in reply to rsc +2
    I do a lot of small projects that require I2C, SPI, and a few GPIO, plus maybe a radio. I almost exclusively use XIAO boards for those. I use Arduino and RPi MCUs a lot less than I used to. The ability…
  • arvindsa
    arvindsa 28 days ago +1
    Arduino started off as a platform to make it easy for people to get started with electronics and they did an amazing job at promoting the ecosystem. There was a board for every level of expertise, all…
  • BigG
    BigG 28 days ago +1
    Here's a real experts opinion on the Arduino Uno Q. As the author notes: " Why build a board this way? Because the two halves are bad at each other's jobs, and every serious embedded Linux project eventually…
Parents
  • Workshopshed
    Workshopshed 16 days ago

    It was Arduino who really got me back into electronics after a few years break.

    It was that combination of ease of getting started, good documentation and good enough software along with a massive library of community libraries, tutorials and examples.

    Having used the Arduino Portenta in its early days, certainly felt the pain of not having those. Both the Portenta and Yun had an internal "bridge" between their two systems but I never felt it worked too well. For example the Yun dumped serial logs onto the bridge during boot.

    I've also used some of the Qualcomm boards such as the DragonBoard, where the advantage of having a more powerful processor and a Linux O/S gives you access to software that already exists for that platform. In my case image recognition via OpenCV.  That was a platform which was a bit more challenging such as having a 1.8v GPIO and 2.0mm spaced sockets. But the documentation and support were good enough for me to complete my project, using an I/O board designed for Raspberry Pi to control the servos.

    So I don't see a big divide between the two and with Arduino getting into the PLCs a few years back, they were already on a path to expand their user base into industry.

    I not too sure about the new boards having having had the challenges above. And for most of my projects the low to medium powered microcontrollers are plenty as long as they can do secure networking. So I do plan to keep using Arduino boards but likely the MKR range as I like the form factor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed 16 days ago

    It was Arduino who really got me back into electronics after a few years break.

    It was that combination of ease of getting started, good documentation and good enough software along with a massive library of community libraries, tutorials and examples.

    Having used the Arduino Portenta in its early days, certainly felt the pain of not having those. Both the Portenta and Yun had an internal "bridge" between their two systems but I never felt it worked too well. For example the Yun dumped serial logs onto the bridge during boot.

    I've also used some of the Qualcomm boards such as the DragonBoard, where the advantage of having a more powerful processor and a Linux O/S gives you access to software that already exists for that platform. In my case image recognition via OpenCV.  That was a platform which was a bit more challenging such as having a 1.8v GPIO and 2.0mm spaced sockets. But the documentation and support were good enough for me to complete my project, using an I/O board designed for Raspberry Pi to control the servos.

    So I don't see a big divide between the two and with Arduino getting into the PLCs a few years back, they were already on a path to expand their user base into industry.

    I not too sure about the new boards having having had the challenges above. And for most of my projects the low to medium powered microcontrollers are plenty as long as they can do secure networking. So I do plan to keep using Arduino boards but likely the MKR range as I like the form factor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur 16 days ago in reply to Workshopshed

    I lived through the MySQL assimilation by Oracle. The developers that made the decision to fork it after the Sun Microsystem aquistion were visionaries.