Arduino Forum Sensor
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
  • Replies 8 replies
  • Subscribers 393 subscribers
  • Views 651 views
  • Users 0 members are here
Related

Sensor

Former Member
Former Member over 9 years ago

I would like to ask if there are any sensors that I could use in detecting the level of powder in a case while reloading. The only thing I can find commercially only tell you when a case is empty or over full. I want to know if it has a level between those two.

1. the level I want

2. anything short of that level

3. anything above that level.

 

any advice would be great thanks

Keith

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +1
    Traditionally the most accurate linear position sensor is an LVDT (linear variable differential transducer) but they can be expensive. A linear potentiometer is a pretty good low-cost alternative. Maybe…
Parents
  • dougw
    dougw over 9 years ago

    Traditionally the most accurate linear position sensor is an LVDT (linear variable differential transducer) but they can be expensive. A linear potentiometer is a pretty good low-cost alternative.

    Maybe you could hook up digital caliper to measure position.

    If you want alarms and extra features, you can connect a digital caliper to a USB port or an arduino for further processing - lots of examples on the net.

    Is it possible to pre-weigh or pre-measure the volume of powder and make a loader or dispenser that loads the correct amount? Like a syringe with graduated markings on the side, or even a mini measuring cup.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago

    Traditionally the most accurate linear position sensor is an LVDT (linear variable differential transducer) but they can be expensive. A linear potentiometer is a pretty good low-cost alternative.

    Maybe you could hook up digital caliper to measure position.

    If you want alarms and extra features, you can connect a digital caliper to a USB port or an arduino for further processing - lots of examples on the net.

    Is it possible to pre-weigh or pre-measure the volume of powder and make a loader or dispenser that loads the correct amount? Like a syringe with graduated markings on the side, or even a mini measuring cup.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 9 years ago in reply to dougw

    Thanks for all the help will  look into the LVDT thanks all

     

    Keith