Arduino Forum Arduino Makefile
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
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 346 views
  • Users 0 members are here
Related

Arduino Makefile

scorpion
scorpion over 9 years ago

I have a zip archive that has a Makefile in it. This archive is code for an arduino, and I want to edit it as an ino, to add to it.

Attachments:
firmwarev12.zip
  • Sign in to reply
  • Cancel

Top Replies

  • kulky64
    kulky64 over 9 years ago +2
    This project is created for bare metal ATtiny85. If you just need to flash this program into a microcontroller, the zip archive contains hex file which you can use to program your ATtiny85 using AVRDUDE…
  • shabaz
    shabaz over 9 years ago +1
    Hi Ben, It looks like conventional C code and a GNU makefile, nothing to do with Arduino. It just happens to build to an Atmel chip, but not using the Arduino software. The .ino file is just a text file…
  • balearicdynamics
    balearicdynamics over 9 years ago +1
    Hi Ben, I agree with shabaz that the parts you can save are the source files. I took a look to the source, the first though was that it was a sort of arduino source from the AVR IDE instead of the more…
Parents
  • kulky64
    kulky64 over 9 years ago

    This project is created for bare metal ATtiny85. If you just need to flash this program into a microcontroller, the zip archive contains hex file which you can use to program your ATtiny85 using AVRDUDE. If you need make changes to this program, you can download WinAVR and Programmers Notepad and edit the files, then recompile it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kulky64
    kulky64 over 9 years ago

    This project is created for bare metal ATtiny85. If you just need to flash this program into a microcontroller, the zip archive contains hex file which you can use to program your ATtiny85 using AVRDUDE. If you need make changes to this program, you can download WinAVR and Programmers Notepad and edit the files, then recompile it.

    • Cancel
    • Vote Up +2 Vote Down