Arduino Forum OLI (Open LCD Interface) a design for using LCD's with Arduino and Raspberry Pie
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
  • Replies 6 replies
  • Subscribers 402 subscribers
  • Views 621 views
  • Users 0 members are here
  • lcd
  • raspeberrypi
  • arduino
Related

OLI (Open LCD Interface) a design for using LCD's with Arduino and Raspberry Pie

jodahm
jodahm over 9 years ago

I have been working on a design to use 5 & 7 inch LCD's with Arduino and Raspberry Pi boards, I have advanced quite a lot and have tested the first prototype, I would like to share this project with this community and open a discussion on the subject

 

https://hackaday.io/project/11447-oli-open-lcd-interface

  • Sign in to reply
  • Cancel

Top Replies

  • jodahm
    jodahm over 9 years ago in reply to Robert Peter Oakes +1
    Well, you are focusing more on only one aspect of the design and not looking the big picture. The idea of this project is to break the lines of the LCD to be driven by any display controller in 3 parts…
Parents
  • dougw
    dougw over 9 years ago

    Great project.

    Are you going to sell your circuit cards or make the designs available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jodahm
    jodahm over 9 years ago in reply to dougw

    I plan to make the project open source, just dont want to release the designs yet, there are minor bugs still on the PCB's and also I want to get some feedback from the community to release a tool that can be used by many makers.

     

    @Douglas: if you are interested on a prototype PCB you can let me know since I had to order a full lot and have just used 2 or 3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jodahm
    jodahm over 9 years ago in reply to dougw

    I plan to make the project open source, just dont want to release the designs yet, there are minor bugs still on the PCB's and also I want to get some feedback from the community to release a tool that can be used by many makers.

     

    @Douglas: if you are interested on a prototype PCB you can let me know since I had to order a full lot and have just used 2 or 3