Arduino Forum Flash programmer for ATmega 168A
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
  • Replies 13 replies
  • Subscribers 401 subscribers
  • Views 2033 views
  • Users 0 members are here
  • flash programmer
  • arduino uno
  • microchip
  • isp
  • atmega168
Related

Flash programmer for ATmega 168A

Former Member
Former Member over 9 years ago

Hello ! I'm going to buy this book http://amzn.com/1449355781 and start to learn programming ATmega 168A in C. In the books component list i found some alternatives for an ISP programmer which you need to programm your microchip. Here are some:

 

1.An Arduino and six wires makes a totally workable flash programmer.        

 

- An original arduino is quite expensive but affordable. Will a fake arduino copy work as a Flash programmer ?

 

 

2.USBTinyISP                                                                                                  

 

- I don't have a soldering iron and not planning to get one for a while.

 

 

3.USBasp, from BaiTe in China                                                                       

 

-In the book it says that i need to flash the firmware into the AVR in the programmer. I don't really know what it means.

 

 

4.USBTiny, tiny version from ehajo.de                                                             

 

- Same as previous option

 

 

5.A homemade programming spider, which plugs into a breadboard around the AVR chip and connects up the programming, power, and reset pins the right way every time. If you’re at all handy with a soldering iron and perfboard, you should make one of these.                    

                                                                                                                        

- Again, i don't have a soldering iron.

 

 

 

I don't know what option to choose. Seems like options 2 and 5 won't work for me att all since i don't have a soldering iron. Options 3 and 4 are not completely clear. Option 1 is the most expensive one but easyest, may be a fake arduino copy would work as a Flash programmer ? I don't know. I would be happy if someone could educate me at this stuff with ISP programmers.

  • Sign in to reply
  • Cancel
Parents
  • beacon_dave
    beacon_dave over 9 years ago

    Ah - very good point - I was assuming that you were planning on using the Arduino IDE.

     

    You can use Atmel Studio to program and AVR Mega. Not sure if it can use the Arduino ISP though. I've used it with the Atmel AVR Dragon programmer/debugger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    Feels like programmer/debugger Atmel ARV Dragon and Atmel Studio feels like more advanced way ! Would it be more profitable to use theese tools to program ATmega ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to Former Member

    Yes, more powerful features available.

     

    The Dragon is a bit more expensive however

    ATAVRDRAGON - ATMEL - IN SYSTEM DEBUGGER / PROGRAMMER, AVR | Farnell element14

     

    Note that the Dragon does not come with a ZIF socket for programming - if you want that then you need to solder one onto it. It does come with a ICSP header similar to the Arduino ISP, so you can connect it to your breadboard project. This is how I've used the Dragon with an ATmega 1284p.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    I'm not sure if i need an advanced board like Atmel ARV Dragon since i'm a complete beginner. But i still have a question if  i can program ATmega with Arduino ISP in C like if you would programm in the Dragon ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to Former Member

    I think the book you are looking at is based around using the AVR GCC compiler which will mean you will likely end up with a hex file that you need to transfer to the ATmega.

     

    You can do this with Atmel Studio and the Dragon via one of the command line tools. It doesn't look like Atmel Studio supports the Arduino ISP as a programmer though, and I don't think you can download a complied binary using Arduino IDE.

     

    Did you take a look at the ATmega168 Xplained Mini ? as that can be programmed directly from Atmel Studio via its USB connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 9 years ago in reply to Former Member

    I think the book you are looking at is based around using the AVR GCC compiler which will mean you will likely end up with a hex file that you need to transfer to the ATmega.

     

    You can do this with Atmel Studio and the Dragon via one of the command line tools. It doesn't look like Atmel Studio supports the Arduino ISP as a programmer though, and I don't think you can download a complied binary using Arduino IDE.

     

    Did you take a look at the ATmega168 Xplained Mini ? as that can be programmed directly from Atmel Studio via its USB connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    Hmm, Xplained Mini seems like a good alternative since i can program Atmega 168 in C with Atmel Studio. Would the book which i'm looking at be helpful in programming ATmega that way ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to Former Member

    I've not read the book so can't really comment. I just had a quick look to see what compiler/programmer it was using.

     

    However I purchased an ATmega328 Xplained mini to follow along with this AVR series:

    https://www.youtube.com/watch?v=UMi6lg563BA&list=PLtQdQmNK_0DRhBWYZ32BEILOykXLpJ8tP&index=1

     

    (You can also use the ATmega168 Xplained mini with that series.

    ATMEGA168PB-XMINI - ATMEL - Evaluation Board, ATmega168Pb Xplained Mini MCU, On-board Debugger, Arduino Shield Compatibl…

    )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    This series of videos was very helpful to me. I'm planing to get the ATmega168 Xplained.