Arduino Forum Flash programmer for ATmega 168A
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
  • Replies 13 replies
  • Subscribers 401 subscribers
  • Views 2068 views
  • Users 0 members are here
  • flash programmer
  • arduino uno
  • microchip
  • isp
  • atmega168
Related

Flash programmer for ATmega 168A

Former Member
Former Member over 9 years ago

Hello ! I'm going to buy this book http://amzn.com/1449355781 and start to learn programming ATmega 168A in C. In the books component list i found some alternatives for an ISP programmer which you need to programm your microchip. Here are some:

 

1.An Arduino and six wires makes a totally workable flash programmer.        

 

- An original arduino is quite expensive but affordable. Will a fake arduino copy work as a Flash programmer ?

 

 

2.USBTinyISP                                                                                                  

 

- I don't have a soldering iron and not planning to get one for a while.

 

 

3.USBasp, from BaiTe in China                                                                       

 

-In the book it says that i need to flash the firmware into the AVR in the programmer. I don't really know what it means.

 

 

4.USBTiny, tiny version from ehajo.de                                                             

 

- Same as previous option

 

 

5.A homemade programming spider, which plugs into a breadboard around the AVR chip and connects up the programming, power, and reset pins the right way every time. If you’re at all handy with a soldering iron and perfboard, you should make one of these.                    

                                                                                                                        

- Again, i don't have a soldering iron.

 

 

 

I don't know what option to choose. Seems like options 2 and 5 won't work for me att all since i don't have a soldering iron. Options 3 and 4 are not completely clear. Option 1 is the most expensive one but easyest, may be a fake arduino copy would work as a Flash programmer ? I don't know. I would be happy if someone could educate me at this stuff with ISP programmers.

  • Sign in to reply
  • Cancel
Parents
  • beacon_dave
    beacon_dave over 9 years ago

    The Arduino ISP programmer comes preassembled - no soldering required.

    https://www.arduino.cc/en/Main/ArduinoISP

    The six pin header is designed to plug directly onto the Arduino ICSP header. However you could use jumper wires to connect it to breadboard if you are working with a stand alone ATmega IC.

     

    ( Adafruit have a little accessory which allows you to use a 6 wire IDC header cable which makes this even easier but it does require soldering.

    https://www.adafruit.com/product/1465

     

    Adafruit also have a breadboard helper which would allow you to plug the ISP directly onto breadboard and this does not require soldering

    https://www.adafruit.com/products/2105  )

     

    Getting started with the ISP

    https://www.arduino.cc/en/Guide/ArduinoISP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    Thanks for your answer, you helped a lot ! So if i buy one of these http://www.atmel.com/devices/atmega168a.aspx and plug them, onto a breadboard I can program it in C with Arduino ISP programmer with no problem and no additional divices ?

     

    I found one copy of arduino ISP on amazon. Would it work as it should ?

    http://amzn.com/B00LUJYI26

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    Thanks for your answer, you helped a lot ! So if i buy one of these http://www.atmel.com/devices/atmega168a.aspx and plug them, onto a breadboard I can program it in C with Arduino ISP programmer with no problem and no additional divices ?

     

    I found one copy of arduino ISP on amazon. Would it work as it should ?

    http://amzn.com/B00LUJYI26