Arduino Forum Flash programmer for ATmega 168A
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
  • Replies 13 replies
  • Subscribers 391 subscribers
  • Views 1884 views
  • Users 0 members are here
  • flash programmer
  • arduino uno
  • microchip
  • isp
  • atmega168
Related

Flash programmer for ATmega 168A

Former Member
Former Member over 9 years ago

Hello ! I'm going to buy this book http://amzn.com/1449355781 and start to learn programming ATmega 168A in C. In the books component list i found some alternatives for an ISP programmer which you need to programm your microchip. Here are some:

 

1.An Arduino and six wires makes a totally workable flash programmer.        

 

- An original arduino is quite expensive but affordable. Will a fake arduino copy work as a Flash programmer ?

 

 

2.USBTinyISP                                                                                                  

 

- I don't have a soldering iron and not planning to get one for a while.

 

 

3.USBasp, from BaiTe in China                                                                       

 

-In the book it says that i need to flash the firmware into the AVR in the programmer. I don't really know what it means.

 

 

4.USBTiny, tiny version from ehajo.de                                                             

 

- Same as previous option

 

 

5.A homemade programming spider, which plugs into a breadboard around the AVR chip and connects up the programming, power, and reset pins the right way every time. If you’re at all handy with a soldering iron and perfboard, you should make one of these.                    

                                                                                                                        

- Again, i don't have a soldering iron.

 

 

 

I don't know what option to choose. Seems like options 2 and 5 won't work for me att all since i don't have a soldering iron. Options 3 and 4 are not completely clear. Option 1 is the most expensive one but easyest, may be a fake arduino copy would work as a Flash programmer ? I don't know. I would be happy if someone could educate me at this stuff with ISP programmers.

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    Hmm, Xplained Mini seems like a good alternative since i can program Atmega 168 in C with Atmel Studio. Would the book which i'm looking at be helpful in programming ATmega that way ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to Former Member

    I've not read the book so can't really comment. I just had a quick look to see what compiler/programmer it was using.

     

    However I purchased an ATmega328 Xplained mini to follow along with this AVR series:

    https://www.youtube.com/watch?v=UMi6lg563BA&list=PLtQdQmNK_0DRhBWYZ32BEILOykXLpJ8tP&index=1

     

    (You can also use the ATmega168 Xplained mini with that series.

    ATMEGA168PB-XMINI - ATMEL - Evaluation Board, ATmega168Pb Xplained Mini MCU, On-board Debugger, Arduino Shield Compatibl…

    )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to beacon_dave

    This series of videos was very helpful to me. I'm planing to get the ATmega168 Xplained.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<