Arduino Forum i have an idea
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
  • Replies 10 replies
  • Subscribers 394 subscribers
  • Views 766 views
  • Users 0 members are here
Related

i have an idea

Former Member
Former Member over 9 years ago

I have a 5 meter fiberglass boat that I've wired all my electronics into but it's not as good as it could be. I have a jre echo sounder, gps, bla bla bla and I don't like it. My thoughts have me scouring YouTube and the internet for an all in 1 unit to replace the big heavy equipment bolted to the cabin roof, I've learnt a tiny bit about the arduino and don't fully understand its capabilities but assume I'm on the right path. I'm wondering if an arduino can be made to display GPS and nmea data like a chart plotter, engine rpm, play music from a smart phone via Bluetooth, switch relays to power an anchor winch, turn on and off lights, touch screen of course. Has anyone attempted or heard of a project like this before or have an idea of where one might start?. I believe this could be a real game changer for anyone with a boat, yacht, PWC or canoe who wants to explore or find a good fishing hole providing they have a 12volt battery. Any advice or help would be helping 100,000 boaties out there wanting an all in 1 reliable unit.

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 9 years ago +1
    i decided to use an old smart phone to start building an app to run and simplify most of what i'm requiring. an arduino will still do the media player and control all the lights i have fitted via bluetooth…
Parents
  • Former Member
    Former Member over 9 years ago

    i decided to use an old smart phone to start building an app to run and simplify most of what i'm requiring. an arduino will still do the media player and control all the lights i have fitted via bluetooth, a second arduino will be fitted to the engine to relay the rpm, temp, gear selection, ect to the touchscreen. So far the app is around 1/3 complete and not as difficult as i thought it'd be... until i have to program the sounder function, will probably replace sounder for goggles and a quick dunk'n over the side of the boat.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago

    i decided to use an old smart phone to start building an app to run and simplify most of what i'm requiring. an arduino will still do the media player and control all the lights i have fitted via bluetooth, a second arduino will be fitted to the engine to relay the rpm, temp, gear selection, ect to the touchscreen. So far the app is around 1/3 complete and not as difficult as i thought it'd be... until i have to program the sounder function, will probably replace sounder for goggles and a quick dunk'n over the side of the boat.