Arduino Forum Mensaje error compilacion Arduino
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
  • Replies 4 replies
  • Subscribers 392 subscribers
  • Views 545 views
  • Users 0 members are here
Related

Mensaje error compilacion Arduino

Former Member
Former Member over 9 years ago

Por favor, me pueden explicar que significan esos mensajes que aparecen cuando se manda compilar un steck en Mint y funciona perfectamente con Windoes ?

 

Arduino:1.6.10 (Linux), Tarjeta:"Arduino/Genuino Uno"

 

SIGILL: illegal instruction

PC=0x8114699

 

goroutine 1 [running, locked to thread]:

math.init·1()

    /usr/local/go/src/math/pow10.go:34 +0x19 fp=0x18435f84 sp=0x18435f80

math.init()

    /usr/local/go/src/math/unsafe.go:21 +0x3f fp=0x18435f88 sp=0x18435f84

strconv.init()

    /usr/local/go/src/strconv/quote.go:455 +0x45 fp=0x18435fa4 sp=0x18435f88

io/ioutil.init()

    /usr/local/go/src/io/ioutil/tempfile.go:95 +0x4a fp=0x18435fc4 sp=0x18435fa4

github.com/go-errors/errors.init()

    /home/jenkins/jenkins/jobs/arduino-builder-linux32/workspace/src/github.com/go-errors/errors/stackframe.go:102 +0x3f fp=0x18435fc8 sp=0x18435fc4

main.init()

    /home/jenkins/jenkins/jobs/arduino-builder-linux32/workspace/src/arduino.cc/arduino-builder/main.go:371 +0x3f fp=0x18435fcc sp=0x18435fc8

runtime.main()

    /usr/local/go/src/runtime/proc.go:58 +0xbd fp=0x18435ff0 sp=0x18435fcc

runtime.goexit()

    /usr/local/go/src/runtime/asm_386.s:2287 +0x1 fp=0x18435ff4 sp=0x18435ff0

 

goroutine 2 [runnable]:

runtime.forcegchelper()

    /usr/local/go/src/runtime/proc.go:90

runtime.goexit()

    /usr/local/go/src/runtime/asm_386.s:2287 +0x1

 

goroutine 3 [runnable]:

runtime.bgsweep()

    /usr/local/go/src/runtime/mgc0.go:82

runtime.goexit()

    /usr/local/go/src/runtime/asm_386.s:2287 +0x1

 

eax     0x23

ebx     0x826e3d8

ecx     0x18400140

edx     0x826e3d8

edi     0x18435f80

esi     0x18435f8c

ebp     0x1843c03d

esp     0x18435f80

eip     0x8114699

eflags  0x210202

cs      0x73

fs      0x0

gs      0x3f

arduino-builder retornó 2

 

Error compilación en tarjeta Arduino/Genuino Uno.

 

Este reporte podría tener más información con

"Mostrar salida detallada durante la compilación"

opción habilitada en Archivo -> Preferencias.

 

 

Muchas gracias

  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 9 years ago

    Instruction bad:

    eip     0x8114699

    Without source, I cannot say more.. But follow the suggestion above:

     

     

    This report may have more information

    "Show detailed output during compilation"

    option enabled File -> Preferences.

    This will turn on better diagnoses.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to clem57

    Estimado, muchas gracias por su pronta respuesta.

    Revisando el fondo de mi mente, opte por desinstalar la vesion que tenia e instalar la 1.6.5-r5 y se acabaron todos los problemas. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to Former Member

    Your welcome. Glad the reinstall fixed the problem. Goes the show that keeping up with later releases fixes bugs in old version.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 9 years ago in reply to Former Member

    Your welcome. Glad the reinstall fixed the problem. Goes the show that keeping up with later releases fixes bugs in old version.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 9 years ago in reply to clem57

    Clem

    Nuevamente muchas gracias por su respuesta, y voy a mantenerme informado de las actualizaciones como usted me sugiere.

    Mis aludos  image