Arduino Forum [Help] Using one BJT(BC637) as switch with Arduino digital pin.
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
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 594 views
  • Users 0 members are here
Related

[Help] Using one BJT(BC637) as switch with Arduino digital pin.

Former Member
Former Member over 9 years ago

Hello, i don't have one reasonable experience with electronics component, and i would like to someone with more experience than me to check if my calculation done right.
First i will control one backlight led that the recommended current draw is 22.7 mA.

Looking up the DC Current Gain on the BC637 datasheet and using the formula Ib = Ic/b i calculated:

Ib = 22.7/25

Ib = 0.908 mA

And arduino logic level is 5V to HIGH and 0V to LOW so i should add a current limiting resistor in series on the BC637 base pin.

So using the formula Rb= (Vcc - Vbe)/Ib i calculated

Rb = (5V - 1V)/0.000908A

Rb is aprox. 4405 ohm

 

So i'm planning to use one 4.7k ohm resistor on Rb  so the backlight should be always less brighter (since less current will flow).

Its my calculation done right? It should work the way i planned?

 

Btw here the simplified schematic

Schematic

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2
    Your close, it is ok to slightly over drive the base as long as you don't exceed its current rating , I cant see the MAX base current in the specs Base − Emitter On Voltage is about 1V max (Typically assumed…
  • Jan Cumps
    Jan Cumps over 9 years ago +1
    The current gain of a transistor is an instable parameter. It will be hard to regulate the current with the transistor alone. it's safer to put a resistor in series with the LED that limits the current…
  • jc2048
    jc2048 over 9 years ago +1
    A BJT is a current amplifier but it's not sensible to work with it directly like that. As Jan Cumps says, the current gain is very variable. It varies from device to device and it is dependent on other…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Your close, it is ok to slightly over drive the base as long as you don't exceed its current rating , I cant see the MAX base current in the specs

    Base − Emitter On Voltage is about 1V max (Typically assumed to be a diode forward voltage of 0.6V so this needs to be subtracted from your formula, you used 1V so that's ok

     

    I would not assume you will get the full 5V out of the CPU but it will be close

     

    So just to be sure the transistor is saturated (Fully turned on so less power dissipated in the transistor, I would reduce the base resistor to 3K3 or 2K8 ish. Basically your using it as a switch, not in its linear region so we want to ensure it is fully on or fully off.

     

    You will also need a current limiting resistor in series with the LED

     

    So 5V - Backlight Volts at 22mA / 22mA to give you series resistor value. There is also probably a certain amount of volts dropped across the Collector / Emitter so if you want it perfect then this should also be factored into your equation

     

    Hope this helps

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Your close, it is ok to slightly over drive the base as long as you don't exceed its current rating , I cant see the MAX base current in the specs

    Base − Emitter On Voltage is about 1V max (Typically assumed to be a diode forward voltage of 0.6V so this needs to be subtracted from your formula, you used 1V so that's ok

     

    I would not assume you will get the full 5V out of the CPU but it will be close

     

    So just to be sure the transistor is saturated (Fully turned on so less power dissipated in the transistor, I would reduce the base resistor to 3K3 or 2K8 ish. Basically your using it as a switch, not in its linear region so we want to ensure it is fully on or fully off.

     

    You will also need a current limiting resistor in series with the LED

     

    So 5V - Backlight Volts at 22mA / 22mA to give you series resistor value. There is also probably a certain amount of volts dropped across the Collector / Emitter so if you want it perfect then this should also be factored into your equation

     

    Hope this helps

    • Cancel
    • Vote Up +2 Vote Down