Arduino Forum Reciprocating Engine Model
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
  • Replies 1 reply
  • Subscribers 391 subscribers
  • Views 245 views
  • Users 0 members are here
  • millis()
  • led
  • servo
  • arduino
Related

Reciprocating Engine Model

maksniil
maksniil over 8 years ago

Guys, I have a reciprocating engine model that involves some movement of 4 parts: A continuous rotation servo, 2 180deg servos and an LED.

This is how it is supposed to move:

The continuous rotation moves at a speed as I specify e.g.: Servo.write(100);

After 2 seconds the first servo moves from 0 deg to 30 deg and then moves back to 30 deg back to 0 deg after 3 seconds.

Then 1 second after the first servo goes back to 0 degrees, the led lights up for 1 second.

2 seconds later the second servo from 0 deg to 30 deg and moves back to 30 to 0 after 3 seconds like the first servo.

 

All of this is executed while the continuous rotation servo is moving without any interruptions or stoppage.

 

Can someone help me please, I need this for my project. Any kind of help will be appreciated.

  • Sign in to reply
  • Cancel
  • clem57
    clem57 over 8 years ago

    Can you give a picture of what you are trying to do? Also what MCU are you using and pins assigned.If built, a schematic could help.

    Clem