Arduino Forum control 250 doors with arduino
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
  • Replies 18 replies
  • Subscribers 392 subscribers
  • Views 1099 views
  • Users 0 members are here
Related

control 250 doors with arduino

abolfazlnejatian
abolfazlnejatian over 8 years ago

Hey Everyone

 

I have a question about my project and I’ll really appreciate any help you can give,

I’m going to programming a software in order to automatically open up 250 doors with FINGERPRINT SCANNER, I mean I’ve 250 members in a gym and I want to recognize any of them by their fingerprint and then open their related door wardrobe.

So the question is, I don’t know after verifying any individual person and understanding the related door, how can I command to the doors to open?

Let me clarify the sentence, Arduino have 16 pins as output and I’ve 250 doors to control.

I know it’s completely ridiculous to dedicate 250 pins to 250 doors but I don’t know how to overcome to this problem and reduce the pins number!

 

Thank you in advance for your attention to this matter.

 

Many thanks

Abolfazl

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 8 years ago +3
    As usual, there are a number of ways to do this type of thing. Perhaps take a look at this tutorial using daisy-chained shift registers: https://www.arduino.cc/en/Tutorial/ShiftOut You could use 5x Arduino…
  • dougw
    dougw over 8 years ago +3
    You can get 256 nodes on an RS485 bus and it can run long distances. It would start with the serial port on your arduino through some RS485 line drivers. http://www.ti.com/lit/an/slla272b/slla272b.pdf…
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    Silly thought: how reliable is a fingerprint recognition system for people who just played basketball, have been swimming or just took a shower after sport? these activities, all common in a gym, alter…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    As usual, there are a number of ways to do this type of thing.

     

    Perhaps take a look at this tutorial using daisy-chained shift registers:

    https://www.arduino.cc/en/Tutorial/ShiftOut

     

    You could use 5x Arduino Mega256 microcontrollers which have significantly more digital IO than an UNO . This may seem ridiculous but could work out easier/cheaper.

     

    Another approach is to move some of the 'intelligence' closer to the locks and use a bus type approach where each lock is given a unique address on the bus and only responds to bus commands with that particular address.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 8 years ago

    As usual, there are a number of ways to do this type of thing.

     

    Perhaps take a look at this tutorial using daisy-chained shift registers:

    https://www.arduino.cc/en/Tutorial/ShiftOut

     

    You could use 5x Arduino Mega256 microcontrollers which have significantly more digital IO than an UNO . This may seem ridiculous but could work out easier/cheaper.

     

    Another approach is to move some of the 'intelligence' closer to the locks and use a bus type approach where each lock is given a unique address on the bus and only responds to bus commands with that particular address.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to beacon_dave

    Dave's last suggestion seems to be the most practical one, if you don't want a wire bundle as thick as a tree's branch.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to Jan Cumps

    That would perhaps depend on where you located the shift registers though. If the lockers are arranged in an XY matrix then you could perhaps space the shift registers at 8-locker intervals along the 'X axis' reducing the wire bundle at any one location considerably.

     

    Same with the distributed microcontroller approach - each ATMega328 microcontroller could service around 20 lockers with digital IO and then use a communications bus between them along the 'X axis'.

     

    Adding the intelligence at each lock may be costly as you have the 250x factor to consider.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to beacon_dave

    A mix-and match approach may be reasonable for both costs and wiring.

    addressable bus devices with enough pins to control a set of doors, placed localy close to these doors. And then a bus line linking all of the bus devices together and to the arduino.

    You'd also have to run a power line and some devices that can switch significant current, because locks are most of the time actuator-controlled. This device can be a relais or an electronic switch.

     

    Because the actuators will generate significant pulses, your bus line has to be resiliant for that. dough suggested a line that can bridge some distance and is relatively forgiving for pulses.

     

    I would't bet on SPI or I2C. They both do well on a pcb, but when you use them with lines of some distance, with 250 possible sources for magnetic pulses (500 sources if the locks are controlled by a relais), chances are dim that it 'll work reliably.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    ... If you route unadressed 'raw' control lines from the arduino, any hacker can get access to all sporter's wallets and iPhones with just two needles and 1 or 2 coin cells. With that, you can put a pulse on every line and see the lockers jump open one by one.