Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Barcode Scanner with Arduino Mega and USB shield
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 416 subscribers
  • Views 1980 views
  • Users 0 members are here
Related

Barcode Scanner with Arduino Mega and USB shield

elizabethmath
elizabethmath over 10 years ago

Hi,

 

I am currently using a barcode scanner to my arduino mega. I use a USB shield to enable my arduino to serve as a USB host for the barcode scanner.

I have found some links online which share the code that I can use.

These codes primarily allow me to enable the barcode scanner as a HID keyboard device.

For some reason , however, the code does not seem compatible with my arduino mega.

I have read on some forums, that some people have this issue when using the code I found on : https://www.youtube.com/watch?v=t5gkg645xGE

 

The example too uses a mega and a barcode of matching compatibility. The choice of USB shield is different.

I simply can not seem to understand what the issue is .

As for my barcode scanner,  it works as it does when I plug it directly into the PC. However, when the beep comes in ( which means its scanned and printed out the output), I cannot trace it. Dont know how and where to find where it is being sent to.

I am currently notified that I have OSC does not start. What exactly does this mean?

 

I was advised by someone to " Just configure one of your hardware serial ports on your mega to read the UART data. " I am really not sure what this means. I was under the impression that the UART was by default transmitted via the hardware serial port.

Does being asked to configure this mean that I need to make changes to my code/ the shield library?

 

Please advice me as to what I can do from here!

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Did you manage to get the code to compile? In the youtube video it shows that there are some errors during the compile stage and then shows how to overcome those errors (coment out some of the includes at the top of the script/sketch)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • elizabethmath
    elizabethmath over 10 years ago in reply to e14 Contributor

    Hi Lucie,

     

    Yes I did.

    The code is exactly the same as what the example finally compiles.

    It compiles fine for me as well.

    Just does not work after that

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • elizabethmath
    elizabethmath over 10 years ago in reply to e14 Contributor

    Hi Lucie,

     

    Yes I did.

    The code is exactly the same as what the example finally compiles.

    It compiles fine for me as well.

    Just does not work after that