Arduino Forum Help adding some kind of heuristic to my relay portion of code
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
  • Replies 9 replies
  • Subscribers 394 subscribers
  • Views 753 views
  • Users 0 members are here
  • arduino uno
Related

Help adding some kind of heuristic to my relay portion of code

toxsickcity
toxsickcity over 8 years ago

Hi all,

 

I have a small issue with my relays switching on and off every second or so, once it hits the temperature.

 

my code controls a arduino uno and using 3 onewire sensors

it controls 1 relay and Red/Blue LED lighting effect for each sensor

 

i have pulled code and added all kinds and to a experienced coder, you will laugh at it.. but it is working so i am happy...

 

 

i would essentially like to setup a somehow instead of having 1 temperature setting, have an upper and lower, instead of being only 30 degrees,

how can i have 30 on and 25 off

this will prevent relay hammer

 

here is the code i need help with...

if (temperature >30) {

digitalWrite(4,HIGH);

} else {

digitalWrite(4,LOW);

}

if (temperature2 >30) {

digitalWrite(8,HIGH);

} else {

digitalWrite(8,LOW);

}

if (temperature3 >30) {

digitalWrite(13,HIGH);

} else {

digitalWrite(13,LOW);

Attachments:
4722.code.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 8 years ago

    What MK wrote will work.  If you want to clean it up in CS terms, have a coupla variables, maybe Cross_Point and Hysteresis, use a formalism.  Then when you want to change these params you won't have to go digging through the code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 8 years ago

    What MK wrote will work.  If you want to clean it up in CS terms, have a coupla variables, maybe Cross_Point and Hysteresis, use a formalism.  Then when you want to change these params you won't have to go digging through the code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to D_Hersey

    The original code the OP wrote should also work.

     

    Any chance you can include all the code as I suspect something else is causing the drop.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxsickcity
    toxsickcity over 8 years ago in reply to mcb1

    Hi mark,

    I did give the else if a go, but seems it didnt help much.. it still hammered.. like on off on off for upto a minute changing state every 1-2 seconds

     

    I would like to simply use original code and use a Minimum time the relay stays on, which will prevent hammer...

     

    I was told to look at this and am confused how to implement this into my code.

     

    /* Blink without Delay
    
     Turns on and off a light emitting diode (LED) connected to a digital
     pin, without using the delay() function.  This means that other code
     can run at the same time without being interrupted by the LED code.
    
     The circuit:
     * LED attached from pin 13 to ground.
     * Note: on most Arduinos, there is already an LED on the board
     that's attached to pin 13, so no hardware is needed for this example.
    
     created 2005
     by David A. Mellis
     modified 8 Feb 2010
     by Paul Stoffregen
     modified 11 Nov 2013
     by Scott Fitzgerald
    
    
     This example code is in the public domain.
    
     http://www.arduino.cc/en/Tutorial/BlinkWithoutDelay
     */
    
    // constants won't change. Used here to set a pin number :
    const int ledPin =  13;      // the number of the LED pin
    
    // Variables will change :
    int ledState = LOW;             // ledState used to set the LED
    
    // Generally, you should use "unsigned long" for variables that hold time
    // The value will quickly become too large for an int to store
    unsigned long previousMillis = 0;        // will store last time LED was updated
    
    // constants won't change :
    const long interval = 1000;           // interval at which to blink (milliseconds)
    
    void setup() {
      // set the digital pin as output:
      pinMode(ledPin, OUTPUT);
    }
    
    void loop() {
      // here is where you'd put code that needs to be running all the time.
    
      // check to see if it's time to blink the LED; that is, if the
      // difference between the current time and last time you blinked
      // the LED is bigger than the interval at which you want to
      // blink the LED.
      unsigned long currentMillis = millis();
    
      if (currentMillis - previousMillis >= interval) {
        // save the last time you blinked the LED
        previousMillis = currentMillis;
    
        // if the LED is off turn it on and vice-versa:
        if (ledState == LOW) {
          ledState = HIGH;
        } else {
          ledState = LOW;
        }
    
        // set the LED with the ledState of the variable:
        digitalWrite(ledPin, ledState);
      }
    }

     

     

    Here is MY CODE image

     

    // HSV fade/bounce for Arduino - scruss.com - 2010/09/12
    // Note that there's some legacy code left in here which seems to do nothing
    // but should do no harm ...
    
    
    #include "OneWire.h"
    //#include "Streaming.h"
    
    
    const int DS18S20a_Pin = 2; //DS18S20 Signal pin on digital 2
    #define MIN_TEMP 10
    #define MAX_TEMP 45
    #define RELAY1  4 // Relay on digital pin 4
    OneWire ds(DS18S20a_Pin);
    
    
    const int DS18S20b_Pin = 7;
    #define MIN_TEMP2 10
    #define MAX_TEMP2 45
    //edit
    #define RELAY2  8
    OneWire dsb(DS18S20b_Pin);
    
    
    const int DS18S20c_Pin = 12;
    #define MIN_TEMP3 10
    #define MAX_TEMP3 45
    //edit
    #define RELAY3  13
    OneWire dsc(DS18S20c_Pin); 
    
    
    
    
    // don't futz with these, illicit sums later
    //#define RED       10// pin for red LED
    //#define RED2       3// pin for red LED
    
    
    #define SIZE    255
    #define SIZE2    255
    #define SIZE3   255
    
    
    #define DELAY    0
    #define DELAY2    0
    #define DELAY3    0
    
    
    #define HUE_MAX  6.0
    #define HUE2_MAX  6.0
    #define HUE3_MAX  6.0
    
    
    #define HUE_DELTA 0.01
    #define HUE2_DELTA 0.01
    #define HUE3_DELTA 0.01
    
    
    int firstPins [] = { 3,5};
    int secondPins [] = { 6,9};
    int thirdPins [] = { 10,11};
    
    
    //int secondPins [] = { 9,10};
    //long deltas[3] = { 5, 6, 7 };
    long rgb[2];
    long rgb2[3];
    long rgb3[3];
    long rgbval;
    long rgbval2;
    long rgbval3;
    // for reasons unknown, if value !=0, the LED doesn't light. Hmm ...
    // and saturation seems to be inverted
    float hue=0.0, saturation=1, value=1;
    float hue2=0.0, saturation2=1, value2=1;
    float hue3=0.0, saturation3=1, value3=1;
    
    
    /*
    chosen LED SparkFun sku: COM-09264
     has Max Luminosity (RGB): (2800, 6500, 1200)mcd
     so we normalize them all to 1200 mcd -
     R  250/600  =  107/256
     G  250/950  =   67/256
     B  250/250  =  256/256
     */
    long bright[2] = { 256, 256};
    long bright2[3] = { 256, 256};
    long bright3[3] = { 256, 256};
    //long bright[3] = { 256, 256, 256};
    
    
    long k, temp_value;
    
    
    void setup () {
      randomSeed(analogRead(4));
      pinMode(RELAY1, OUTPUT);
      Serial.begin(57600);
      for (k=0; k<2; k++) {
        pinMode(firstPins[k], OUTPUT);
        rgb[k]=0;
         analogWrite(firstPins[k], rgb[k] * bright[k]/256);
      }
      randomSeed(analogRead(4));
        pinMode(RELAY2, OUTPUT);
      Serial.begin(57600);
      for (k=0; k<2; k++) {
        pinMode(secondPins[k], OUTPUT);
        rgb2[k]=0;
        analogWrite(secondPins[k], rgb[k] * bright[k]/256);
      }
      randomSeed(analogRead(4));
        pinMode(RELAY3, OUTPUT);
      Serial.begin(57600);
      for (k=0; k<2; k++) {
        pinMode(thirdPins[k], OUTPUT);
        rgb3[k]=0;
        analogWrite(thirdPins[k], rgb[k] * bright[k]/256);
      }
    }
    //temperature1
    void loop() {
      pinMode(RELAY1, OUTPUT); //new
       pinMode(RELAY2, OUTPUT); //new
       pinMode(RELAY3, OUTPUT); //new
      float temperature = constrain(getTemp(), MIN_TEMP, MAX_TEMP);
      float temperature2 = constrain(getTemp2(), MIN_TEMP2, MAX_TEMP2);
      float temperature3 = constrain(getTemp3(), MIN_TEMP3, MAX_TEMP3);
      float deltaTemp = (MAX_TEMP - MIN_TEMP);
      float deltaTemp2 = (MAX_TEMP2 - MIN_TEMP2);
      float deltaTemp3 = (MAX_TEMP3 - MIN_TEMP3);
      float deltaHue = 4 - 0;
      float deltaHue2 = 4 - 0;
      float deltaHue3 = 4 - 0;
      hue = map((temperature - MIN_TEMP) * 100, 0, deltaTemp * 100, deltaHue * 100, 0) / 100.0;
      hue2 = map((temperature2 - MIN_TEMP2) * 100, 0, deltaTemp2 * 100, deltaHue2 * 100, 0) / 100.0;
      hue3 = map((temperature3 - MIN_TEMP3) * 100, 0, deltaTemp3 * 100, deltaHue3 * 100, 0) / 100.0;
      //Serial << "Temperature: " << temperature << endl;
      //Serial << "HUE: " << hue << endl;
      rgbval=HSV_to_RGB(hue, saturation, value);
      rgbval2=HSV_to_RGB2(hue2, saturation2, value2);
      rgbval3=HSV_to_RGB3(hue3, saturation3, value3);
      
      rgb[0] = (rgbval & 0x00FF0000) >> 16; // there must be better ways
      rgb[1] = (rgbval & 0x0000ff00) >> 8;
     // rgb[2] = rgbval & 0x000000FF; 
    for (k=0; k<2; k++) { // for all three colours
        analogWrite(firstPins[k], rgb[k] * bright[k]/256);}
    
    
      rgb2[0] = (rgbval2 & 0x00ff0000) >> 16; // there must be better ways
     rgb2[1] = (rgbval2 & 0x0000ff00) >> 8;
     // rgb2[1] = rgbval2 & 0x0000ff00;
       for (k=0; k<2; k++) { // for all three colours
            analogWrite(secondPins[k], rgb2[k] * bright[k]/256);}
    
      rgb3[0] = (rgbval3 & 0x00ff0000) >> 16; // there must be better ways
     rgb3[1] = (rgbval3 & 0x0000ff00) >> 8;
     // rgb2[1] = rgbval2 & 0x0000ff00;
       for (k=0; k<2; k++) { // for all three colours
            analogWrite(thirdPins[k], rgb3[k] * bright[k]/256);}
    
        //delay(DELAY);
    if (temperature < 40) {
    digitalWrite(4,HIGH);
    } else {
    digitalWrite(4,LOW);
    }
    
    
    if (temperature2 > 40) {
    digitalWrite(8,HIGH);
    } else {
    digitalWrite(8,LOW);
    }
    if (temperature3 > 40) {
    digitalWrite(13,HIGH);
    } else {
    digitalWrite(13,LOW);
    }
    }
    
    
    // sensor1
    float getTemp(){
     //returns the temperature from one DS18S20 in DEG Celsius
    
    
     byte data[12];
     byte addr[8];
    
    
     if ( !ds.search(addr)) {
       //no more sensors on chain, reset search
       ds.reset_search();
       return -10;
     }
     if ( OneWire::crc8( addr, 7) != addr[7]) {
       Serial.println("CRC is not valid!");
       return -10;
     }
     if ( addr[0] != 0x10 && addr[0] != 0x28) {
       Serial.print("Device is not recognized");
       return -10;
     }
    
    
     ds.reset();
     ds.select(addr);
     ds.write(0x44,1); // start conversion, with parasite power on at the end
    
    
     byte present = ds.reset();
     ds.select(addr);  
     ds.write(0xBE); // Read Scratchpad
    
    
    
     for (int i = 0; i < 9; i++) { // we need 9 bytes
      data[i] = ds.read();
     }
    
     ds.reset_search();
    
     byte MSB = data[1];
     byte LSB = data[0];
    
    
     float tempRead = ((MSB << 8) | LSB); //using two's compliment
     float TemperatureSum = tempRead / 16;
    
     return TemperatureSum;
    }
    
    
    //2nd sensor
    
    
    float getTemp2(){
     //returns the temperature from one DS18S20 in DEG Celsius
    
    
     byte data[12];
     byte addr[8];
    
    
     if ( !dsb.search(addr)) {
       //no more sensors on chain, reset search
       dsb.reset_search();
       return -10;
     }
    
    
     if ( OneWire::crc8( addr, 7) != addr[7]) {
       Serial.println("CRC is not valid!");
       return -10;
     }
    
    
     if ( addr[0] != 0x10 && addr[0] != 0x28) {
       Serial.print("Device is not recognized");
       return -10;
     }
    
    
     dsb.reset();
     dsb.select(addr);
     dsb.write(0x44,1); // start conversion, with parasite power on at the end
    
    
     byte present = dsb.reset();
     dsb.select(addr);  
     dsb.write(0xBE); // Read Scratchpad
    
    
    
     for (int i = 0; i < 9; i++) { // we need 9 bytes
      data[i] = dsb.read();
     }
    
     dsb.reset_search();
    
     byte MSB2 = data[1];
     byte LSB2 = data[0];
    
    
     float temp2Read = ((MSB2 << 8) | LSB2); //using two's compliment
     float Temperature2Sum = temp2Read / 16;
    
     return Temperature2Sum;
    }
    
    
    //3nd sensor
    
    
    float getTemp3(){
     //returns the temperature from one DS18S20 in DEG Celsius
    
    
     byte data[12];
     byte addr[8];
    
    
     if ( !dsc.search(addr)) {
       //no more sensors on chain, reset search
       dsc.reset_search();
       return -10;
     }
    
    
     if ( OneWire::crc8( addr, 7) != addr[7]) {
       Serial.println("CRC is not valid!");
       return -10;
     }
    
    
     if ( addr[0] != 0x10 && addr[0] != 0x28) {
       Serial.print("Device is not recognized");
       return -10;
     }
    
    
     dsc.reset();
     dsc.select(addr);
     dsc.write(0x44,1); // start conversion, with parasite power on at the end
    
    
     byte present = dsc.reset();
     dsc.select(addr);  
     dsc.write(0xBE); // Read Scratchpad
    
    
    
     for (int i = 0; i < 9; i++) { // we need 9 bytes
      data[i] = dsc.read();
     }
    
     dsc.reset_search();
    
     byte MSB3 = data[1];
     byte LSB3 = data[0];
    
    
     float temp3Read = ((MSB3 << 8) | LSB3); //using two's compliment
     float Temperature3Sum = temp3Read / 16;
    
     return Temperature3Sum;
    }
    
    
    // End Sensors
    
    
    long HSV_to_RGB( float h, float s, float v ) {
      /* modified from Alvy Ray Smith's site: http://www.alvyray.com/Papers/hsv2rgb.htm */
      // H is given on [0, 6]. S and V are given on [0, 1].
      // RGB is returned as a 24-bit long #rrggbb
      int i;
      float m, n, f;
    
    
      // not very elegant way of dealing with out of range: return black
      if ((s<0.0) || (s>1.0) || (v<1.0) || (v>1.0)) {
        return 0L;
      }
    
    
      if ((h < 0.0) || (h > 6.0)) {
        return long( v * 255 ) + long( v * 255 ) * 256 + long( v * 255 ) * 65536;
      }
      i = floor(h);
      f = h - i;
      if ( !(i&1) ) {
        f = 1 - f; // if i is even
      }
      m = v * (1 - s);
      n = v * (1 - s * f);
      switch (i) {
      case 6:
      case 0: 
        return long(v * 255 ) * 65536 + long( n * 255 ) * 256 + long( m * 255);
      case 1: 
        return long(n * 255 ) * 65536 + long( v * 255 ) * 256 + long( m * 255);
      case 2: 
        return long(m * 255 ) * 65536 + long( v * 255 ) * 256 + long( n * 255);
      case 3: 
        return long(m * 255 ) * 65536 + long( n * 255 ) * 256 + long( v * 255);
      case 4: 
        return long(n * 255 ) * 65536 + long( m * 255 ) * 256 + long( v * 255);
      case 5: 
        return long(v * 255 ) * 65536 + long( m * 255 ) * 256 + long( n * 255);
      }
    }
    //hsv 2
    long HSV_to_RGB2( float h, float s, float v ) {
      /* modified from Alvy Ray Smith's site: http://www.alvyray.com/Papers/hsv2rgb.htm */
      // H is given on [0, 6]. S and V are given on [0, 1].
      // RGB is returned as a 24-bit long #rrggbb
      int i;
      float m, n, f;
    
    
      // not very elegant way of dealing with out of range: return black
      if ((s<0.0) || (s>1.0) || (v<1.0) || (v>1.0)) {
        return 0L;
      }
    
    
      if ((h < 0.0) || (h > 6.0)) {
        return long( v * 255 ) + long( v * 255 ) * 256 + long( v * 255 ) * 65536;
      }
      i = floor(h);
      f = h - i;
      if ( !(i&1) ) {
        f = 1 - f; // if i is even
      }
      m = v * (1 - s);
      n = v * (1 - s * f);
      switch (i) {
      case 6:
      case 0: 
        return long(v * 255 ) * 65536 + long( n * 255 ) * 256 + long( m * 255);
      case 1: 
        return long(n * 255 ) * 65536 + long( v * 255 ) * 256 + long( m * 255);
      case 2: 
        return long(m * 255 ) * 65536 + long( v * 255 ) * 256 + long( n * 255);
      case 3: 
        return long(m * 255 ) * 65536 + long( n * 255 ) * 256 + long( v * 255);
      case 4: 
        return long(n * 255 ) * 65536 + long( m * 255 ) * 256 + long( v * 255);
      case 5: 
        return long(v * 255 ) * 65536 + long( m * 255 ) * 256 + long( n * 255);
      }
    }
    //hsv 3
    long HSV_to_RGB3( float h, float s, float v ) {
      /* modified from Alvy Ray Smith's site: http://www.alvyray.com/Papers/hsv2rgb.htm */
      // H is given on [0, 6]. S and V are given on [0, 1].
      // RGB is returned as a 24-bit long #rrggbb
      int i;
      float m, n, f;
    
    
      // not very elegant way of dealing with out of range: return black
      if ((s<0.0) || (s>1.0) || (v<1.0) || (v>1.0)) {
        return 0L;
      }
    
    
      if ((h < 0.0) || (h > 6.0)) {
        return long( v * 255 ) + long( v * 255 ) * 256 + long( v * 255 ) * 65536;
      }
      i = floor(h);
      f = h - i;
      if ( !(i&1) ) {
        f = 1 - f; // if i is even
      }
      m = v * (1 - s);
      n = v * (1 - s * f);
      switch (i) {
      case 6:
      case 0: 
        return long(v * 255 ) * 65536 + long( n * 255 ) * 256 + long( m * 255);
      case 1: 
        return long(n * 255 ) * 65536 + long( v * 255 ) * 256 + long( m * 255);
      case 2: 
        return long(m * 255 ) * 65536 + long( v * 255 ) * 256 + long( n * 255);
      case 3: 
        return long(m * 255 ) * 65536 + long( n * 255 ) * 256 + long( v * 255);
      case 4: 
        return long(n * 255 ) * 65536 + long( m * 255 ) * 256 + long( v * 255);
      case 5: 
        return long(v * 255 ) * 65536 + long( m * 255 ) * 256 + long( n * 255);
      }
    }

     

    Cheers

     

    I noticed my code here is older, I have few issues such as the > and < in the relay part, the first is different to temperature2 and temperature3

     

    I will Dump a new code when I get home, sorry for this confusing anyone haha