Arduino Forum Help adding some kind of heuristic to my relay portion of code
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
  • Replies 9 replies
  • Subscribers 394 subscribers
  • Views 753 views
  • Users 0 members are here
  • arduino uno
Related

Help adding some kind of heuristic to my relay portion of code

toxsickcity
toxsickcity over 8 years ago

Hi all,

 

I have a small issue with my relays switching on and off every second or so, once it hits the temperature.

 

my code controls a arduino uno and using 3 onewire sensors

it controls 1 relay and Red/Blue LED lighting effect for each sensor

 

i have pulled code and added all kinds and to a experienced coder, you will laugh at it.. but it is working so i am happy...

 

 

i would essentially like to setup a somehow instead of having 1 temperature setting, have an upper and lower, instead of being only 30 degrees,

how can i have 30 on and 25 off

this will prevent relay hammer

 

here is the code i need help with...

if (temperature >30) {

digitalWrite(4,HIGH);

} else {

digitalWrite(4,LOW);

}

if (temperature2 >30) {

digitalWrite(8,HIGH);

} else {

digitalWrite(8,LOW);

}

if (temperature3 >30) {

digitalWrite(13,HIGH);

} else {

digitalWrite(13,LOW);

Attachments:
4722.code.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago

    At first glance there are a few things that are not right.

     

    Line 99 you define the relay outputs  pinMode(RELAY1, OUTPUT);

    However you haven't declared what pin Relay1 is attached to.

     

    same again for Line 107, and 115.

     

    I don't think declaring the outputs in the loop section is a good idea.

    While you can change between an input and output the state of the pin at the time may change.

     

    It has the comment /new after it so I presume it was an attempt to overcome why it was cycling.

     

    At line 167 you are changing the state of Pins 4, 8 and 13, which presumably have the relays attached.

    But these pins are not declared as Outputs, and will not be getting driven with the full current.

     

    Your declaration (void setup() ) also has some extras.

    Lines 98, 106, 114 are the same and it only needs 1.

    Lines 100, 108, 116 also are the same, again only 1 reqd.

     

    I think there is some work also necessary on the getTemp routines.

    You seem to do a search and reset at each time you call the routine.

    In practice you really need to do the search, and then make the call to read the temperature.

    For some readings it can take upto 750mS, so I always set it up to do the call and then check if 1 sec has gone, and keep coming back.

     

    I suspect that this may be why the relays are dropping out.

    basically the call to read temp is returning a vause that is not within the range, and therefore it is dropping out (as it should).

     

     

    You could prove that by adding these lines at line 165

    Serial.print("temperature = ");

    Serial.println(temperature);

    Serial.print("temperature2 = ");

    Serial.println(temperature2);

    Serial.print("temperature3 = ");

    Serial.println(temperature3);

     

    When you run it select Serial Monitor (set speed to 57600 to match line 100)

    It will display the readings.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago

    At first glance there are a few things that are not right.

     

    Line 99 you define the relay outputs  pinMode(RELAY1, OUTPUT);

    However you haven't declared what pin Relay1 is attached to.

     

    same again for Line 107, and 115.

     

    I don't think declaring the outputs in the loop section is a good idea.

    While you can change between an input and output the state of the pin at the time may change.

     

    It has the comment /new after it so I presume it was an attempt to overcome why it was cycling.

     

    At line 167 you are changing the state of Pins 4, 8 and 13, which presumably have the relays attached.

    But these pins are not declared as Outputs, and will not be getting driven with the full current.

     

    Your declaration (void setup() ) also has some extras.

    Lines 98, 106, 114 are the same and it only needs 1.

    Lines 100, 108, 116 also are the same, again only 1 reqd.

     

    I think there is some work also necessary on the getTemp routines.

    You seem to do a search and reset at each time you call the routine.

    In practice you really need to do the search, and then make the call to read the temperature.

    For some readings it can take upto 750mS, so I always set it up to do the call and then check if 1 sec has gone, and keep coming back.

     

    I suspect that this may be why the relays are dropping out.

    basically the call to read temp is returning a vause that is not within the range, and therefore it is dropping out (as it should).

     

     

    You could prove that by adding these lines at line 165

    Serial.print("temperature = ");

    Serial.println(temperature);

    Serial.print("temperature2 = ");

    Serial.println(temperature2);

    Serial.print("temperature3 = ");

    Serial.println(temperature3);

     

    When you run it select Serial Monitor (set speed to 57600 to match line 100)

    It will display the readings.

     

    Cheers

    Mark