Arduino Forum Temp Sensor question..
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
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 869 views
  • Users 0 members are here
Related

Temp Sensor question..

medictrode
medictrode over 8 years ago

Hello all,

 

I am trying to teach my 9 y/o how to do basic coding, and I figured the Arduino UNO was a good place to start. The problem is I am no coder, but I wish I had someone just to show me something like this when I was this age so I wouldn't be so dumb to it. So along with blinking LEDs, and showing cause and effect from changing Parameters I decided a Temp/Humidity sensor would be fun and easy for us. Obviously I got my code from around the net and made mild changes,so any credit goes to the original coder.

 

We added an LCD screen in and managed to make it work. The problem is the LCD screen won't update temp/Hum unless a client is connected. I think I've figured out why with the "if(client.available())" line. I get that it would read if no browser is connected, however I am not smart enough to code my way around it. I've tried moving the sensor reads to other areas and all I've gotten is various errors.. Any help would be super appreciated, and sorry for the Newb question as I am learning, as is the little one..

 

 

 

/*-----( Import needed libraries )-----*/

#include <SPI.h>

#include <Ethernet.h>

#include <dht.h>

#include <Wire.h>

#include <LiquidCrystal.h>

 

 

/*-----( Declare Constants and Pin Numbers )-----*/

#define DHT11_PIN 9  // The Temperature/Humidity sensor

LiquidCrystal lcd(3, 4, 5, 6, 7, 8);

 

 

// Enter a MAC address and IP address for your controller below.

// The IP address will be dependent on your local network:

byte mac[] = {

  0xBA, 0xDB, 0x00, 0xBF, 0xFE, 0xED };

 

 

/*-----( Declare objects )-----*/

IPAddress ip(192,168,15,69);

 

 

// Initialize the Ethernet server library

// with the IP address and port you want to use

// (port 80 is default for HTTP):

EthernetServer server(80);

 

 

dht DHT;  //The Sensor Object

/*-----( Declare Variables )-----*/

 

 

 

 

 

 

void setup()   /****** SETUP: RUNS ONCE ******/

{

  lcd.begin(16, 2);

  // Open serial communications and wait for port to open:

  Serial.begin(9600);

  while (!Serial) {

    ; // wait for serial port to connect. Needed for Leonardo only

  }

 

 

 

 

  // start the Ethernet connection and the server:

  Ethernet.begin(mac, ip);

  server.begin();

  Serial.print("server is at ");

  Serial.println(Ethernet.localIP());

 

 

 

}//--(end setup )---

 

 

 

 

void loop()   /*----( LOOP: RUNS OVER AND OVER AGAIN )----*/

 

 

 

 

{

 

  // listen for incoming clients

  EthernetClient client = server.available();

  if (client) {

    Serial.println("new client");

    // an http request ends with a blank line

    boolean currentLineIsBlank = true;

    while (client.connected()) {

      if (client.available()) {

        char c = client.read();

        Serial.write(c);

        // if you've gotten to the end of the line (received a newline

        // character) and the line is blank, the http request has ended,

        // so you can send a reply

        if (c == '\n' && currentLineIsBlank) {

          // send a standard http response header

          client.println("HTTP/1.1 200 OK");

          client.println("Content-Type: text/html");

          client.println("Connnection: close");

          client.println();

          client.println("<!DOCTYPE HTML>");

          client.println("<html>");

          // add a meta refresh tag, so the browser pulls again every 5 seconds:

          client.println("<meta http-equiv=\"refresh\" content=\"5\">");

          client.print("<TITLE>  Temp Sensor</TITLE>");

          client.print("<center><H1 style=color:blue>TEMPERATURE SENSOR :-) </H1>");  

          client.println("<br />");  

          client.println("<br />"); 

           client.println("<br />");

 

 

          /*----(Get sensor reading, calculate and print results )-----------------*/

 

 

          int chk = DHT.read11(DHT11_PIN);

 

 

          Serial.print("Read sensor: ");

          switch (chk)

          {

          case 0:

            Serial.println("OK");

            break;

          case -1:

            Serial.println("Checksum error");

            break;

          case -2:

            Serial.println("Time out error");

            break;

          default:

            Serial.println("Unknown error");

            break;

          } 

 

 

          client.print("Temperature (C): ");

          client.println((float)DHT.temperature, 1); 

          client.println("<br />"); 

           client.println("<br />");

         

          

         

          client.print("Temperature (F): ");

          client.println(Fahrenheit(DHT.temperature), 1);

          client.println("<br />");

          client.println("<br />");

        

       

         

          client.print("Humidity (%): ");

          client.println((float)DHT.humidity, 0); 

          client.println("<br />");

         client.println("<br />");

         

 

 

          client.print("Temperature (K): ");

          client.println(Kelvin(DHT.temperature), 1);

          client.println("<br />"); 

          client.println("<br />"); 

 

 

          client.print("Dew Point (F): ");

          client.println(dewPoint(DHT.temperature, DHT.humidity));

          client.println("<br />");

         client.println("<br />");  

 

 

          client.print("Dew PointFast (C): ");

          client.println(dewPointFast(DHT.temperature, DHT.humidity));

          client.println("<br />");

         client.print("<br />");

     

       lcd.clear();

        lcd.setCursor(0,0);

        lcd.print("Temp: ");

        lcd.print(Fahrenheit( DHT. temperature));

        lcd.print(" F");

       lcd.setCursor(0,1);

         lcd.print("Hum:  ");

         lcd.print((float)DHT.humidity);

         lcd.print(" %");

        

 

 

 

 

          /*--------( End Sensor Read )--------------------------------*/

          client.println("</html>");

          break;

        }

    

        if (c == '\n') {

          // you're starting a new line

          currentLineIsBlank = true;

        }

        else if (c != '\r') {

          // you've gotten a character on the current line

          currentLineIsBlank = false;

        }

      }

    }

    // give the web browser time to receive the data

    delay(1);

    // close the connection:

    client.stop();

    Serial.println("client disonnected");

  }

} // END Loop

 

 

/*-----( Declare User-written Functions )-----*/

//

//Celsius to Fahrenheit conversion

double Fahrenheit(double celsius)

{

  return celsius * 1.8 + 32;

}

 

 

//Celsius to Kelvin conversion

double Kelvin(double celsius)

{

  return celsius + 273.15;

}

 

 

// dewPoint function NOAA

// reference: http://wahiduddin.net/calc/density_algorithms.htm

double dewPoint(double celsius, double humidity)

{

  double A0= 373.15/(273.15 + celsius);

  double SUM = -7.90298 * (A0-1);

  SUM += 5.02808 * log10(A0);

  SUM += -1.3816e-7 * (pow(10, (11.344*(1-1/A0)))-1) ;

  SUM += 8.1328e-3 * (pow(10,(-3.49149*(A0-1)))-1) ;

  SUM += log10(1013.246);

  double VP = pow(10, SUM-3) * humidity;

  double T = log(VP/0.61078);   // temp var

  return (241.88 * T) / (17.558-T) * 1.8 + 32;

 

 

 

 

 

 

 

}

 

 

// delta max = 0.6544 wrt dewPoint()

// 5x faster than dewPoint()

// reference: http://en.wikipedia.org/wiki/Dew_point

double dewPointFast(double celsius, double humidity)

{

  double a = 17.271;

  double b = 237.7;

  double temp = (a * celsius) / (b + celsius) + log(humidity/100);

  double Td = (b * temp) / (a - temp);

  return Td;

 

 

 

 

 

 

 

 

}

 

 

/* ( THE END ) */

  • Sign in to reply
  • Cancel

Top Replies

  • medictrode
    medictrode over 8 years ago +2
    Thank you all for the replies, super appreciated. I suppose I wasn't clear, and I apologize for that. I built the circuit first to work off of a web interface, and it worked well. I also decided the LCD…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to medictrode +2
    That's perfectly possible. To do that, move the LCD code out of these loops while (client.connected()) { if (client.available()) { } }
  • Jan Cumps
    Jan Cumps over 8 years ago +1
    This example requires that your Arduino is connected to a network, with an ethernet shield. It seems that this example also requires that a server is running on address 192.168.15.69 that listens to commands…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    This example requires that your Arduino is connected to a network, with an ethernet shield.

     

    It seems that this example also requires that a server is running on address 192.168.15.69 that listens to commands from your Arduino.

    Or that the Arduino is that server itself, and the 192.xxx is the network address of the Arduino?

    Did you get additional info with the sample code that documents that?

     

    If you only want to read the sensor and display on the LCD, remove all lines in the code that refer to:

    ethernet, mac, client, IP.

    you will also have to remove the matching closing brackets when you remove a WHILE or IF line.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 8 years ago

    This example requires that your Arduino is connected to a network, with an ethernet shield.

     

    It seems that this example also requires that a server is running on address 192.168.15.69 that listens to commands from your Arduino.

    Or that the Arduino is that server itself, and the 192.xxx is the network address of the Arduino?

    Did you get additional info with the sample code that documents that?

     

    If you only want to read the sensor and display on the LCD, remove all lines in the code that refer to:

    ethernet, mac, client, IP.

    you will also have to remove the matching closing brackets when you remove a WHILE or IF line.