Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum ROBOTDYN card. Mega + WiFi R3 ATmega2560 + ESP8266 (8 Mb mémoire)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 429 subscribers
  • Views 8764 views
  • Users 0 members are here
Related

ROBOTDYN card. Mega + WiFi R3 ATmega2560 + ESP8266 (8 Mb mémoire)

serge28
serge28 over 9 years ago

bonjour,

je viens d'acquérir une carte de ce type, achetée sur internet " https://fr.aliexpress.com/item/Mega-WiFi-R3-ATmega2560-ESP8266-8Mb-memory-USB-TTL-CH340G-Compatible-for-Arduino-Mega-Nod… , " malheureusement c'est nouveau et il est impossible de trouver des exemples ou plus d'information concernant des exemples de sketch.

J'ai pu constater en faisant des test, que la partie ESP8266 fonctionne, de même que la carte Mega.

Mais je suis incapable de faire communiquer les deux ensembles, comme il semble que c'est prévu par le "Serial 3"

 

Pourriez vous m'aider ?

Merci par avance
Serge

  • Sign in to reply
  • Cancel

Top Replies

  • bissa
    bissa over 9 years ago +1
    This work for me: Configure the dip switch in the "special" mode: 1(on) 2(on) 3(on) 4(on) 5(off) 6(off) 7(off) 8(off) Turn the switch in RXD3 run the following schech, after adjusting SSID and PASSWORD…
  • kimleng
    kimleng over 8 years ago in reply to isotopa +1
    do u have other way to cmmnicate like facebook or telegeam that is easy to discuss?
  • isotopa
    isotopa over 8 years ago in reply to isotopa +1
    Entiendo. para ejecutar mega + wifi al mismo tiempo, primero debes programar esp8266 y mega antes. Cada uno con sus jumpers. Aquí les dejo un manual: Para probar el funcionamiento de la placa, es necesario…
Parents
  • serge28
    serge28 over 9 years ago

    Hi,

    I did some try too with Blynk, but i didn't used the "stand alone example". For me it can't be considered as "Alone"  ....except if u want us the ESP itself only

    I think it will be better t to consider the ESP as Arduino shield, connected.

    Honnestly, i didn't succed even on this way image ... refered to "Userbin" chat upper, we have all, problems to make both connecting.

    If u find urself some solutions, i will be glad to read about it.


    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • serge28
    serge28 over 9 years ago

    Hi,

    I did some try too with Blynk, but i didn't used the "stand alone example". For me it can't be considered as "Alone"  ....except if u want us the ESP itself only

    I think it will be better t to consider the ESP as Arduino shield, connected.

    Honnestly, i didn't succed even on this way image ... refered to "Userbin" chat upper, we have all, problems to make both connecting.

    If u find urself some solutions, i will be glad to read about it.


    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • serge28
    serge28 over 9 years ago in reply to serge28

    I found this comment too on the china web site i bought it :

     

    "The description states very precisely how to use the dip switches on this board for the different modes. The most important mode and the only reason why I bought this board is to use the Mega together with the ESP to be able to connect the Mega with the WWW. This mode DOES NOT work. It is possible to use the Mega and the ESP separately but NOT together. This makes the price for this board extremely high because the single components are cheaper. Due to the testing I had to perform I missed the dead line to open a dispute."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kimleng
    kimleng over 8 years ago in reply to serge28

    Serge de Chazelles@ we have the same problem..but now did you solved it yet?  If you  can work fine with it...Could you please share us? Thank you.