Arduino
  • Products
  • More
Arduino
Arduino Forum ROBOTDYN card. Mega + WiFi R3 ATmega2560 + ESP8266 (8 Mb mémoire)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 430 subscribers
  • Views 8503 views
  • Users 0 members are here
Related

ROBOTDYN card. Mega + WiFi R3 ATmega2560 + ESP8266 (8 Mb mémoire)

serge28
serge28 over 9 years ago

bonjour,

je viens d'acquérir une carte de ce type, achetée sur internet " https://fr.aliexpress.com/item/Mega-WiFi-R3-ATmega2560-ESP8266-8Mb-memory-USB-TTL-CH340G-Compatible-for-Arduino-Mega-Nod… , " malheureusement c'est nouveau et il est impossible de trouver des exemples ou plus d'information concernant des exemples de sketch.

J'ai pu constater en faisant des test, que la partie ESP8266 fonctionne, de même que la carte Mega.

Mais je suis incapable de faire communiquer les deux ensembles, comme il semble que c'est prévu par le "Serial 3"

 

Pourriez vous m'aider ?

Merci par avance
Serge

  • Sign in to reply
  • Cancel

Top Replies

  • bissa
    bissa over 9 years ago +1
    This work for me: Configure the dip switch in the "special" mode: 1(on) 2(on) 3(on) 4(on) 5(off) 6(off) 7(off) 8(off) Turn the switch in RXD3 run the following schech, after adjusting SSID and PASSWORD…
  • kimleng
    kimleng over 8 years ago in reply to isotopa +1
    do u have other way to cmmnicate like facebook or telegeam that is easy to discuss?
  • isotopa
    isotopa over 8 years ago in reply to isotopa +1
    Entiendo. para ejecutar mega + wifi al mismo tiempo, primero debes programar esp8266 y mega antes. Cada uno con sus jumpers. Aquí les dejo un manual: Para probar el funcionamiento de la placa, es necesario…
Parents
  • trial&error
    trial&error over 9 years ago

    I have the very same device and the very same problem. I read all the information I could find on this device and I tried all the code but I only can us it as a normal Arduino Mega. I have no clue on how to get the ESP8266 working.

    Did somebody made some progress on this in the meantime or do u just use it as a  really overpriced Arduino Mega? image

     

    Whren I try the code mentioned above I get following error:

    <command-line>:0:9: error: expected identifier before numeric constant

    C:\Users\...\Documents\Arduino\libraries\arduino-ESP8266-master/ESP8266.h:69:7: note: in expansion of macro 'ESP8266'

    class ESP8266 : public Stream

           ^

    <command-line>:0:9: error: expected unqualified-id before numeric constant

    C:\Users\...\Documents\Arduino\libraries\arduino-ESP8266-master/ESP8266.h:69:7: note: in expansion of macro 'ESP8266'

    class ESP8266 : public Stream

           ^

    exit status 1

     

    I have my board set to "Generic ESP8266 Module" as mentioned here: MEGA+WiFi R3 ATmega2560+ESP8266, flash 32MB, USB-TTL CH340G, Micro-USB

    but also set to Arduino Mega I get a different Error Message:

    MEGA_WiFi:6: error: no matching function for call to 'ESP8266::ESP8266(HardwareSerial&, long int)'

     

    MEGA_WiFi:18: error: no matching function for call to 'ESP8266::getVersion()'

     

    MEGA_WiFi:20: error: 'class ESP8266' has no member named 'setOprToStation'

     

    MEGA_WiFi:30: error: 'class ESP8266' has no member named 'getLocalIP'

     

    no matching function for call to 'ESP8266::ESP8266(HardwareSerial&, long int)'

     

    Does somebody now how to fix this? I am getting really frustrated at not progressing at my project image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • trial&error
    trial&error over 9 years ago

    I have the very same device and the very same problem. I read all the information I could find on this device and I tried all the code but I only can us it as a normal Arduino Mega. I have no clue on how to get the ESP8266 working.

    Did somebody made some progress on this in the meantime or do u just use it as a  really overpriced Arduino Mega? image

     

    Whren I try the code mentioned above I get following error:

    <command-line>:0:9: error: expected identifier before numeric constant

    C:\Users\...\Documents\Arduino\libraries\arduino-ESP8266-master/ESP8266.h:69:7: note: in expansion of macro 'ESP8266'

    class ESP8266 : public Stream

           ^

    <command-line>:0:9: error: expected unqualified-id before numeric constant

    C:\Users\...\Documents\Arduino\libraries\arduino-ESP8266-master/ESP8266.h:69:7: note: in expansion of macro 'ESP8266'

    class ESP8266 : public Stream

           ^

    exit status 1

     

    I have my board set to "Generic ESP8266 Module" as mentioned here: MEGA+WiFi R3 ATmega2560+ESP8266, flash 32MB, USB-TTL CH340G, Micro-USB

    but also set to Arduino Mega I get a different Error Message:

    MEGA_WiFi:6: error: no matching function for call to 'ESP8266::ESP8266(HardwareSerial&, long int)'

     

    MEGA_WiFi:18: error: no matching function for call to 'ESP8266::getVersion()'

     

    MEGA_WiFi:20: error: 'class ESP8266' has no member named 'setOprToStation'

     

    MEGA_WiFi:30: error: 'class ESP8266' has no member named 'getLocalIP'

     

    no matching function for call to 'ESP8266::ESP8266(HardwareSerial&, long int)'

     

    Does somebody now how to fix this? I am getting really frustrated at not progressing at my project image