Arduino Forum Is it Save To Use Servos With Just An Arduino?
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
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 824 views
  • Users 0 members are here
  • servo
Related

Is it Save To Use Servos With Just An Arduino?

davidhaw
davidhaw over 8 years ago

I have bad experiences with using a motor and frying my Arduino, so is it save to use servos with an Arduino with no diodes? If yes, why?

  • Sign in to reply
  • Cancel
  • rachaelp
    rachaelp over 8 years ago

    Hi David,

     

    The servo should be fine. I'm assuming you are planning to power the servo from an external power source in which case you are just sending a control signal to the servo from the Arduino and this is just driving into the control circuitry of the servo itself.

     

    It might be interesting to work out why you are damaging your Arduino when using motors. How are you connecting up the motor? Are you putting in any protection to deal with back EMF when the motor is turned off?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidhaw
    davidhaw over 8 years ago in reply to rachaelp

    I forgot to use a diode. Didn't know if it was safe when I saw people using servos without a diode and just an Arduino.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidhaw
    davidhaw over 8 years ago in reply to rachaelp

    Also the project with the servo is here: Servo Motor Control with an Arduino

     

    In this project they didn't use a external power supply like you suggested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to davidhaw

    My reason for mentioning using an external power supply was simply because it wasn't stated what the servo was and I being cautious in case you were using a big servo which had significant current draw which might overload the regulator on the Arduino. There is a motor inside the servo but I would expect them to deal with back EMF inside the servo itself otherwise the internal control circuit would likely get fried.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davidhaw
    davidhaw over 8 years ago in reply to rachaelp

    The Servo I'm using is tiny. It is a Tower Pro Micro Servo 9G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • teprojects1
    teprojects1 over 8 years ago

    Yeah buddy, It's safe and more reliable. Even you can check my engineering projects in which I used arduino to control the speed of servo and its movements.