Arduino Forum I need help with an arduino project
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
  • Replies 5 replies
  • Subscribers 394 subscribers
  • Views 622 views
  • Users 0 members are here
  • arduino
Related

I need help with an arduino project

theroguephoenix
theroguephoenix over 8 years ago

I am currently trying to run a servo, and four LED's on an Arduino nano, as well as giving it a remote via separate Arduino nano, Joystick, and nrf24l01 attached to both. Can anyone help me set up a code, and perhaps a pin diagram to make my dream a reality? I need the LED's to turn on, as well as the servo moving from 0 to 30 degrees when the button on the joystick is pressed. If you need anymore information feel free to ask, and I'll explain as best I can. I am VERY new to Arduino and need some expert help.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +2
    RF Control System For R/C Vehicle Based On Arduino And nRF24L01
  • bleckman74
    bleckman74 over 8 years ago in reply to teprojects1 +1
    Or There is a Bunch of HELPFUL People at Know How's G+ Community, there are 11,000 Experts that can and WILL answer your question if you watch Twit.TV There is a Show Called "KNOW HOW" Its hosted by Fr…
Parents
  • dougw
    dougw over 8 years ago

    RF Control System For R/C Vehicle Based On Arduino And nRF24L01

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    RF Control System For R/C Vehicle Based On Arduino And nRF24L01

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • theroguephoenix
    theroguephoenix over 8 years ago in reply to dougw

         Let's say I was going to make 2 sets of LED's, two for the eyes, and the second set would contain two different colored LED's for the eyes, as well as one in the mouth of the creature I am trying to make. Would it be possible to have it to where the first set would turn on with the first click of the joystick, and the second set for the eyes, as well as the LED in the mouth, would active on the second click, while turning the first set off? What I am trying to build is a skull with eyes that will light up blue, but when activated the second set of eyes turn on being bright white instead. This skull also has a servo in the jaw that, when the joystick is pressed twice,  would go to 30 degrees and then back to 0 after a delayed time, as well as light up the LED in the mouth once it opens. I'm not advanced enough to know how to write that code myself, or even get the grounds to where my LED's don't interfere with the nRF24l01. One ground pin is used as well as the vin to power the nano via LiPo, so I only have one ground pin left over. I'm sorry if this is alot, but you can see why I need assistance.