Arduino Forum pure sine wave inverter using arduino
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
  • Replies 4 replies
  • Subscribers 394 subscribers
  • Views 1418 views
  • Users 0 members are here
  • arduion
Related

pure sine wave inverter using arduino

teprojects1
teprojects1 over 8 years ago

I want to design pure sine wave inverter using Arduino I found the code of pure sine wave inverter using pic microcontroller but I need code with arduino. Can you help me write code with arduino.

Thanks..

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +2
    I think you will find the Arduino (ATMEGA328) is not fast enough for this purpose, there are a lot of calculations and control algorithms needed to do this reliably and with quality If your not bound to…
Parents
  • balearicdynamics
    balearicdynamics over 8 years ago

    Hello Junad,

     

    I took a look to the project link for PIC. It sounds almost well documented so porting is not so difficult and sure you can find here helpful hints and suggestions, from me but not me only.

    Indeed I suggest you should plan to put some more effort than only asking... Maybe good if you explain your project in detail, did you have already setup a minimal hardware design (e.g. based on the half bridge as shown in the project you mention)?

    PIC project is just pure C and it is not difficult at least to try to see what does this code do... Did you tried to copy-and-paste the source in the Arduino ide to see what happens? First of all you should isolate the bare C algorithms and formulas, defines and constants that will work almost the same on Arduino then see about the hardware specific differences ...

     

    I suppose you have not posted this discussion hoping that someone past you the code you are searching for ...

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 8 years ago

    Hello Junad,

     

    I took a look to the project link for PIC. It sounds almost well documented so porting is not so difficult and sure you can find here helpful hints and suggestions, from me but not me only.

    Indeed I suggest you should plan to put some more effort than only asking... Maybe good if you explain your project in detail, did you have already setup a minimal hardware design (e.g. based on the half bridge as shown in the project you mention)?

    PIC project is just pure C and it is not difficult at least to try to see what does this code do... Did you tried to copy-and-paste the source in the Arduino ide to see what happens? First of all you should isolate the bare C algorithms and formulas, defines and constants that will work almost the same on Arduino then see about the hardware specific differences ...

     

    I suppose you have not posted this discussion hoping that someone past you the code you are searching for ...

     

    Enrico