Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need to find a load cell for Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 418 subscribers
  • Views 2775 views
  • Users 0 members are here
  • weight to analog value
  • measuring
  • load cells
  • dynamics weight detection
  • weight sensor
  • weight
Related

Need to find a load cell for Arduino

balearicdynamics
balearicdynamics over 9 years ago

Hello.

I am searchng for a cheap sensor that can analog detect weight differences to do something like a scale. The weight range should be about 5 Kg max and about 0.250 min. I have searched for load cells but I have only found extremely expensive components so I have the suspect I am looking in the wrong direction. I am aware that in load cells the precision factor is almost constant so if the same cell can be used in a range of 1-10 Gr with a precision of 1/100 (I mean 0.01 g) the same cell measuring the range of 1-5 Kg the precision remain the same (or comparable). This is not a very influencing factor as it is most important to detect the weight vs time variation: I need to detect a weight variation in the order of less than 0.5 seconds and a continuous slow variation.

 

Any help will be appreciated. I know the principle but unfortunately in my past experience I have only worked with 10-1000 tons weight cells (always controlled by something like Arduino) and this is not the case.

 

Enrico

 

Update

Also a flexible sensor or force sensor can be useful to make this project. But also in this case I have not found reliable products, only (unreliable) flexysensors on baggood or from some small selles. I am searching flexible sensors (possible alternative) as well as load cells for cheap by a provider that can sell it as components. Not just kits, shields etc...

 

Message was updated by: Enrico Miglino

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 9 years ago +3
    Hello, just two ideas: have you considered dismantling a kitchen scale / personal scale to find out, how is the weight measured? How about using some air bumper with an air pressure sensor? David
  • michaelkellett
    michaelkellett over 9 years ago in reply to balearicdynamics +3
    You can pay anything you like for load cells. A decent one, certified for retail selling applications in the UK will cost about £15 (15kg range) in decent numbers (10k per annum). But you can buy a cheapo…
  • mcb1
    mcb1 over 9 years ago +3
    If I recall fvan used one in his Forget Me Not Challenge [CaTS] ForgetMeNot - 3D Printing: Weighing scale mark
Parents
  • mcb1
    mcb1 over 9 years ago

    If I recall fvan used one in his Forget Me Not Challenge

    [CaTS] ForgetMeNot - 3D Printing: Weighing scale

     

    mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to mcb1

    Hello Mark, I saw the post, it's very inspiring and he followed something very similar what I have in mind. Thank you for the suggestion

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fvan
    fvan over 9 years ago in reply to balearicdynamics

    Love it when old posts remain useful (and someone remembers they exist!)  image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to fvan

    I always adopt the useful practice of bookmarking. And also searching in posts as one of the first sources of my knowledge base (when the search works well) image

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to fvan

    I always adopt the useful practice of bookmarking. And also searching in posts as one of the first sources of my knowledge base (when the search works well) image

     

    Enrico