Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using Speaker Wire with breadboard
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 415 subscribers
  • Views 1148 views
  • Users 0 members are here
Related

Using Speaker Wire with breadboard

vandia
vandia over 9 years ago

Hi, I got some 20ga stranded speaker wire at Wal-Mart. I can strip it to 18 guage but it doesn't seem to want to hold. Trying to solder it, maybe I'm just shabby at it, but I can't get it to hold into the breadboard.

 

I was wondering if there's some form of pin-crimps that allow you to put breadboard pin headers to wire?

 

Also, I wanted to find out if anyone objected to the idea of using this wire for what i'm using it for: To connect 5v ultrasonic distance sensors to my breadboard. I'm using one speaker wire for 5v/gnd, and another for trig/echo. Is there any reason why I should not use this (eg: stranded maybe causing resistance issues with some sensors if I switch to analog?)

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Vandia, I like to use the same technique as shabaz . I also like to solder small pieces of leads from components to the ends of wires and put heat shrink over the solder joint to provide some strain…
  • shabaz
    shabaz over 9 years ago +2
    Hi vandia, I take it you plan to use the speaker wire to connect sensors quite far away? There are pin crimps but then you need to buy a crimp tool as well, and you'll end up with a heavy gauge wire on…
Parents
  • shabaz
    shabaz over 9 years ago

    Hi vandia,

     

    I take it you plan to use the speaker wire to connect sensors quite far away?

    There are pin crimps but then you need to buy a crimp tool as well, and you'll end up with a heavy gauge wire on the breadboard and it could slip out of the holes due to its weight.

    Another approach (neater I think) is to buy male-to-male jumper cablesmale-to-male jumper cables and chop them in half, and solder them to the ends of your speaker wire, and put some heat-shrink insulation around the join. It would look tidy and would be a lightweight cable to your breadboard.

     

    Or, an even cheaper solution is to just solder sacrificial resistors to the ends of the cable, and chop off the resistor, leaving a tinned copper wire attached to your speaker cable. Use heat-shrink sleeving on it as before. But I think the jumper cable method is better.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago

    Hi vandia,

     

    I take it you plan to use the speaker wire to connect sensors quite far away?

    There are pin crimps but then you need to buy a crimp tool as well, and you'll end up with a heavy gauge wire on the breadboard and it could slip out of the holes due to its weight.

    Another approach (neater I think) is to buy male-to-male jumper cablesmale-to-male jumper cables and chop them in half, and solder them to the ends of your speaker wire, and put some heat-shrink insulation around the join. It would look tidy and would be a lightweight cable to your breadboard.

     

    Or, an even cheaper solution is to just solder sacrificial resistors to the ends of the cable, and chop off the resistor, leaving a tinned copper wire attached to your speaker cable. Use heat-shrink sleeving on it as before. But I think the jumper cable method is better.